2022-02-10 9:03 AM
If I call SUBGRF_SetRx() with a timeout of, let's say 100 ticks in LoRa mode, I don't get an RX timeout IRQ at the end of the timeout.
I have checked the radio status with SUBGRF_GetStatus(). The radio goes to RX then back to standby.
I have cross-checked that SUBGRF_SetDioIrqParams() is called so RX timeout IRQ is enabled.
I have cross-checked that SUBGHZ_Radio_IRQHandler is enabled (indeed it is called after a TX).
In the datasheet the RX/TX timeout IRQ is indicated as valid for GFSK and LORA mode.
I realize that the drivers manage the radio timeouts in LoRa mode with timers, not with the radio abilities. So what I am trying to do is not covered by the examples.
Do I miss something?
2022-07-26 12:57 AM
Hi,
I have same problem.
Have you solved this problem yet?
If you solved this problem, please tell me how to fix this problem.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.