NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I'm working with the STM32WB5MMG module and have been using SPI communication with DMA successfully. Previously, in a bare-metal setup, the following was working perfectly:HAL_SPI_TransmitReceive_DMA() starts the transferHAL_SPI_TxRxCpltCallback() is...
Hi, we are designing a product around the STM32WB5MMGH6TR but cannot find a full datasheet.On the product page we can find what is described as a datasheet (main purple download button at the top) but is only a 37 pages "technical brochure" that does...
I am new to the NUCLEO WL55JC1 and wanted to experiment with LoRaWAN.I've followed the YT series on the topic, especially the 3rd part (https://www.youtube.com/watch?v=8KNfrWoa1fw&t=26s). My End node is properly joined and connected to the things net...
Hello everyone, I am strugling with a STM32WB5MMGH that I am using with transparent mode. I am using the STM32WB5MMGH on a custom board with a STM32L4R9VIT6. The goal of the project is to use the STM32WB5 as a bridge to send data from a smartphone ap...
Please tell me how to enable FTD in X-CUBE-MATTER. Is it possible to have it function as a Thread Router?
Hi everyone, im using an STM32WB and i just managed to get my own BLE<->UART bridge to "half work".But my problem is about UART managing.If i receive data with length of less than 247bytes(set by me) just stays in the rx bufer and no DMA transfer com...
Hello everyone, I'm writing in search of some help, as I'm not sure what else to check. I have just built a custom board controlled by an STM32WBA65RIV6, and I'm trying to connect it via DFU mode. Everything seems to be set up correctly, but the devi...
Hello,I would like to build a project using a STM32WL33 µC on IAR Embedded Workbench IDE v9.30.1. Unfortunately, this version of IAR does not support this µC and I would like to import it but i cannot find any package suitable for IAR. Do you have an...
I'm implementing "User defined skeleton" application. I correctly join to gateway and server chirpstack is logging 'join accept', 'join_request. When i can send some data to server i get 2 errors from library Lorawan, 'LORAMAC_HANDLER_ERROR' in funct...
I cannot get STM32WLE5 (on a RAK3172 module) to exit from stop mode on either RTC timer or rising EXTI pin. I'm using STM Cube HAL functions and the stm32_lpm_if.c library. I have tried pin PB3 as either EXTI3 or as PWR_WKUP3. If I use EXTI3, I set ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.