STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WBA65 USB Phy Clock power usage

Hello,I am working with an STM32WBA65RI that is on our custom board, and working to reduce our power usage. Along this journey I found the issue with the HAL_PCD_MspInit() / DeInit() where the logic for the RCC PWR was inverted, which was another pos...

JFisherLegato_1-1761241661788.png JFisherLegato_0-1761240882377.png

stm32wba65, BLE and RTC timer not firing

I have a set of BLE characteristics set up, and working ok. The project uses FreeRTOS. I want to be able to have the stm32wba65 sleep in low power, then wake up at a specific time of day. After wakeup,I have a 5-second RTOS timer to take a series of ...

SLevi.1 by Senior
  • 395 Views
  • 0 replies
  • 0 kudos

Nucleo WL55JC2 - Generate continuous 432.492 MHz

Hi,I’m looking for some help — I’m trying to generate a continuous waveform at 432.492 MHz using the Nucleo WL55JC2, but I haven’t had any success so far. I also tried at 861.1 MHz, but still got no output.After extensive troubleshooting, I discovere...

Franck95 by Associate
  • 544 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.