STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Rdp = 1, locks backup register

I’m working on an STM32WLE5 device and I’m facing a reproducible issue when enabling Read-Out Protection level 1 (RDP = 1). When RDP = 0, everything works as expected: i can write/read RTC Backup registers, my initialization sequence behaves correctl...

Resolved! B-WL5M-SUBG1 (STM32WL5MOC) current consumption too high

Hello,We have an issue with the B-WL5M-SUBG1 evaluation board: The idle current consumption is higher than expected: 89 uA (vs. expected: 1-2 uA) after joining (OTAA) successfully.Board: B-WL5M-SUBG1Firmware: STM32CubeWL/Projects/B-WL5M-SUBG1/Applica...

JBive.1 by Associate III
  • 3822 Views
  • 7 replies
  • 2 kudos

Resolved! Sigfox and LoRa AT commands for STM32WL5MOC

The STM32WL5MOC component is both LoRaWAN and Sigfox verified. I need to be able to use both types of connections. AT commands for LoRaWAN are readily available. Is there a guide of AT commands for Sigfox and an AT command to switch between modes? Th...

Resolved! STM32WL5MOC power consumption

Hello,I'm looking to measure the power consumption of the STM32WL5MOC component on a B-WL5M-SUBG1 development board.I'm looking for the power consumption announced by the Sleep Mode datacheet (140nA - 810nA).I connected directly to JP2 to use only ST...

alexemdesgagne_0-1712602977112.png

Boot problem in STM32WLE5

Hello ST, We are using the STM32WLE5 controller in our product.The system always works on 1.8V. Based on demand, we switch to 3.3V and fallback to 1.8V.Our product is IoT-based, charged through solar to a supercapacitor.The main problem is that the c...

kalpeshDryad_0-1763066406831.png IMG_6364.jpg

Resolved! STM32WBA54 SAI Slave mode DMA cannot stop and reinitiate

STM32WBA54 SAI work in slave mode with DMA: SAI1_Block_A Slave out, SAI1_Block_B Slave in. test code as:  MX_SAI1_Init();//in  __HAL_LINKDMA(&hsai_BlockB1, hdmarx, handle_GPDMA1_Channel2);  MX_RxQueue_Config();  HAL_DMAEx_List_SetCircularMode(&RxQueu...

HuangFan by Associate II
  • 678 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.