NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello ST Community Team. First of all, I want to thank you for the new AI plug-in. It is really helpful specially will looking for informations on the STM32 documents. We hope to have the same for other ST products. About the Typo, on the Table 1 of ...
Hi everyone,I'm working with a custom board based on the STM32WB55, and I'm facing a very strange issue with the Bluetooth Low Energy advertising. BLE advertising works perfectly when the board is running under debugger (SWD debug mode), wireless sta...
I want to put my STM32WB05 into sleep mode and utilize the Bluetooth wakeup feature to wake it up. I have not found much information about this online, and was curious if it can be set up in the IOC or if it needs to be added manually?
I am trying to debug code for Nucleo-WL55JC1 board using sample code from the STM website. It is the LoRAWAN_End _Node. I complies fine and creates .elf file. However when a try do download with the STM32Cube I get the following error: An internal...
I would like to use the STM32WL33 as a radio receiver and continuously transfer all I/Q samples to my computer for further processing.Also, I want to use the highest possible IQ sampling rate (CHF_E = 0, 500k IQ samples per second = 64 Mbit/s).I've ...
Hello,I am working with the STM32WL55CC (48-pin package). When I imported the official STM32CubeWL example projects from ST, I noticed that they provide both SINGLE CORE and DUAL CORE versions. But the board that these examples are listed under STM32...
Hello,I recently updated my CubeMX version from v6.14.1 to the latest, and am no longer able to open the .ioc file. Selecting "continue", results in attempting to unzip DB.6.0.141.tar.bz2 where it hangs until failing.Selecting "migrate" results in th...
Hi ST community,I wanted to develop BLE application using the nucleo stm32wb55rg and the zephyr project v4.3.0. what i did is take a nucleo stm32wb55rg board first i upgraded the FUS from the STM32Cube/Repository/STM32Cube_FW_WB_V1.23.0/Projects/STM3...
I am getting the same problem with my nucleowb05kz board
Hello,I’m new to ST boards and currently working with an STM32WB09.My goal is to make the board recognized as a BLE HID Gamepad, including an analog joystick.To get started, I used the HID Mouse example from the library.I managed to modify the HID re...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.