2024-04-08 12:10 PM
Hello,
I'm looking to measure the power consumption of the STM32WL5MOC component on a B-WL5M-SUBG1 development board.
I'm looking for the power consumption announced by the Sleep Mode datacheet (140nA - 810nA).
I connected directly to JP2 to use only STM and I supply 3.6V and I measure the consumption with Otii software and an Otii Arc Pro.
I measured a cosomation of 112uA, far from what I should have.
Do you have a method for measuring sleep mode power consumption?
Thanks for your help.
Solved! Go to Solution.
2024-04-09 12:27 PM
2024-04-09 12:27 PM
Hi
We finally figured out our problem.
Thanks!
2024-05-28 2:39 AM
Hello,
We have a similar issue: The minimum current consumption is higher than expected: 89 uA (expected: 1-2 uA) after joining (OTAA) successfully.
Do you have an idea what could be the issue?
Board: B-WL5M-SUBG1
Firmware: STM32CubeWL/Projects/B-WL5M-SUBG1/Applications/LoRaWAN/LoRaWAN_AT_Slave
Version: STM32CubeWL V1.3.0 (latest from https://github.com/STMicroelectronics/STM32CubeWL)
Power supply: 5 V via CN4 (E5V)
Current measurement: IDD jumper (JP2) using Joulescope
Thanks!
2024-05-28 7:05 AM
This post is closed. Could you please create a new one. Also, could you please give more details about your issue.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-28 7:22 AM
Sure, see new post
Thanks!
2025-11-14 3:14 AM - edited 2025-11-14 3:15 AM
Hello there,
Could you post references or method you used for this sleep application could you kindly share it over here
Regards,
Prasadh
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.