2024-05-28 7:18 AM
Hello,
We have an issue with the B-WL5M-SUBG1 evaluation board: The idle current consumption is higher than expected: 89 uA (vs. expected: 1-2 uA) after joining (OTAA) successfully.
Do you have an idea what could be the issue?
Thanks!
Solved! Go to Solution.
2024-05-28 10:39 AM
Hi,
To resolve this issue, we pull the UART TX and RX pins high.
Maybe that could help you.
Alexandre
2024-05-28 7:29 AM
Could you please add the details of the configurations that you are doing.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-28 7:48 AM
Hi, steps to reproduce the issue:
Thanks!
2024-05-28 10:39 AM
Hi,
To resolve this issue, we pull the UART TX and RX pins high.
Maybe that could help you.
Alexandre
2024-05-29 2:43 AM
Hello Alexandre,
Thank you very much for your hint, you nailed it!
We changed two things:
This way, the idle current consumption went down to 1.9 uA! We are very happy with this.
Details:
Projects/B-WL5M-SUBG1/Applications/LoRaWAN/LoRaWAN_AT_Slave/Core/Src/usart.c: change:
GPIO_InitStruct.Pin = USARTx_RX_Pin|USARTx_TX_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP; // <-- changed
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF8_LPUART1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);Projects/B-WL5M-SUBG1/Applications/LoRaWAN/LoRaWAN_AT_Slave/Core/Src/gpio.c: add in function MX_GPIO_Init():
/* Configure GPIO pin : JTDI */
GPIO_InitStruct.Pin = GPIO_PIN_15;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);The same changes can be applied to Projects/B-WL5M-SUBG1/Applications/LoRaWAN/LoRaWAN_End_Node as well.
Thanks again!
2024-05-29 5:16 AM
Excellent!
Happy to hear this news!
Alexandre
2025-11-14 3:21 AM
Hello there,
Did you use any specfic sleep modes to achieve this or just the above mentioned steps kindly let me know of the configurations and references you have used for achieveing this, I am planning on a low power use case for that chip too.
Thanks in Advance!
Regards,
Prasadh
2025-11-17 12:40 AM
Hello Prasadh,
We used the above mentioned steps, nothing more. Does this answer your question?
BR
Jonas
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.