STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

I want to configure B-L072Z-LRWAN1 Board-1 to transmit data through USB device(CDC) and another board-2 to receive data through LoRa, if board-2 after receiving data, if it send some data then board-1(which is connected to PC) have to receive it.

Between Board 1 and Board 2 data exchange should be done through LoRa and data exchange between Board 1 and PC should be through USB. It would be very helpful if someone help with this.

Error: failed to erase memory

I'm using LoRa E5 mini board that has STM32WLE5 MCU on it.I use STM32CubeProgrammer and the STlink of a Nucleo64 board to send the firmware to it.For some boards, I cannot succeed to flash them and get this error : When I try to use STM32CubeIDE I've...

0693W00000Y8XmyQAF.png 0693W00000Y8XncQAF.png
Hugo_VOLA by Associate II
  • 5292 Views
  • 3 replies
  • 0 kudos

What is the device behavior when operating near the maximum junction temperature? Specifically what is/are the failure mode(s)? Leakage current? Latch-up? Die melt?

Have an application for STM32WB55 which is likely to be occasionally exposed to 125C (max) ambient, but with very low power consumption. What is the behavior at the allowed limit? Do leakage currents increase dramatically (leading to thermal runawa...

KHepp.1 by Associate
  • 1498 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.