STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

WB5x CDC com port issue

Hi, I have a problem with USB CDC on STM32WB55CE,My Project version is v1.13.& ble stack(stm32wb5x_BLE_Stack_basic_fw V1.15.0)it's all good on WB55CG(1M)but when I use WB55CE(512K)my CDC can work with no ble stack,and it will failure with stack, My c...

YDong.3 by Associate
  • 1692 Views
  • 2 replies
  • 1 kudos

No longer able to build projects from STM32CubeIDE.

I get the following error when I attempt to Build or Clean any project.21:36:49 **** Build of configuration Debug for project BLE_HeartRate **** make -j12 all "make -j12 all" terminated with exit code -1073741515. Build might be incomplete.   21:36:...

HCohe.1 by Associate III
  • 6274 Views
  • 4 replies
  • 2 kudos

Problems with CAN comunication to STM32WL using MCP2515

Hy, I'm currently working on a project that requires CAN and that information needs to be sent via wireless, for that reason, I chose the NUCLEO stm32WL board. To make the CAN work I have to use the MCP2515 module, that converts CAN to SPI so that th...

FPicc.1 by Senior
  • 3731 Views
  • 2 replies
  • 0 kudos

Hi, I am using the STM32WB55 custom board as a client. My Task is to create a connection with the server when a button is pressed. and send the write attribute command and then disconnect from the server immediately.

Steps I am following:Scan for the server and get the MAC of the serverWhen the button is pressed call aci_gap_create_connection to start the connectionThen write the attribute and disconnect from the server.Hear the problem I am facing is it takes 3s...

AM.12 by Associate III
  • 2020 Views
  • 5 replies
  • 0 kudos

Using STM32WB for bidirectional smartphone application

I developed a prototype using a UART to Bluetooth dongle, the HC-05. This worked like a charm. I could pair my smartphone to it and continuously send data between the MCU Board and my smartphone. Now I want to optimize size and cost, therefore I choo...

YGail.2 by Associate III
  • 1853 Views
  • 2 replies
  • 2 kudos

STM32WB for low latency wireless mouse application

As the title says, I want to create a wireless mouse and was wondering if it was possible to make a low latency mouse using two STM32WBs (one for the mouse and one for the computer). Is this possible with this MCU series or is it better to use a dedi...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.