NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello.I'm trying to run this LoRaWAN FUOTA code: github.com/ SylvainMontagny/STM32WL/tree/main/STM32WL_FUOTA (that's the Single-core project on the Application Note AN5554), but i get the following error:c:\st\stm32cubeide_1.9.0\stm32cubeide\plugins\...
I am a hobbyist that only has basic oscilloscope and function generator that is (according to AN5042) not accurate enough to tune the HSE crystal. Is the HSE crystal in the NUCLEO-WB55RG pre-tuned?
I have tried running the BLE_HeartRate application as generated by STM32CubeIDE v1.11.0 which used WB FV 1.15.0. I am running on a custom board (DK board is not available right now) that has a STM32WB5MMG module, the recommended capacitors, and a he...
If I write to address 0, it prevents from entering shutdown mode.The vector table is relocated to code.As far as I understand, writing to address 0 in this case is not illegal. For sure it does not generates a fault.The following code enters shutdown...
Hi, I would like to try nucleo-WL55 in LoRa Node with Quatz and see temperature influence in RF signal.So I have unsolder R2, and solder R39/R40. But now LoRaWAN_AT_Slave does not work anymore, even if I change TCXO to Quartz in .ioc file. I can see ...
Hi everybody!Working on Martian Robot développed by VittaScience, I need to read values coming from 5 blackline sensors to the ADC of the wb55.I tried to analogRead() the pin but nothing...Some ideas? Thanks!
I am currently trying to read the value from a characteristic after detecting that the user has written to it. I am calling aci_gatt_read_char_value() which is returning 0 (BLE success). From here I am expecting an event which triggers the aci_att_r...
Voice is heard through the codec chip, but the noise is severe.There is no noise when you listen to the voice from the PC through the USB output.I don't know if the SAI setting on the Central is wrong or the codec chip setting is wrong. If you playba...
It looks as if the RNG is made unavailable to the M4 when the M0 has booted the BLE stack. This looks to be true because I can initialize and use the RNG before starting the BLE stack. Once I launch C2, the RNG registers read as zeros.Is this a req...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.