NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi, I'm trying to start the zigbee on Nucleo-WB55.After upgrading the FUS to 1.2.0.0 and Stack to 1.16.0.0 without any problem, I get an issue in the running code when it checks the "StackType",it should be 48 or 49 but it returns 0:Tested with two ...
Hi All,I have implemented a code using Arduno IDE. In that we are transmitting data at every 5 minutes. For that I am getting sleep current around 6uA. But When I am using STM32cubeIDE to generate same type of code I am getting sleep current around 5...
HelloI have a P-NUCLEO-LRWAN3 kit. I would like to apply some peripheral at Gateway but I didn't find the source code.If I can't get the gateway source code. I would like to get the binary pre-installed on the NUCLEO-WRWAN3 gateway.Thank you.
Hi, I want to choose a ST MCU/MPU and I would like the CPU to have BLE, to be able to run a low power mode (STANDBY), use < 5µA in STANDBY and be able to listen on BLE during STANDBY mode Best is that BLE chip would be in STANDBY as well but listen...
How to write our own STM32WB BD Address when production? Is there any tool or APIs of Windows to control STM32WB for testing frequency offset/ TX power/ RX sensitivity with 8852.
I'm using a NUCLEO-WB55RG board and if I create a new project in STM32CubeIDE 1.12.0 and enable the STM32_WPAN and HeartRate example it doesn't work because the different buffers that need to be in SRAM2 is not placed there.The app_entry.c defines th...
Hi All,I have implemented EEPROM Emul Middleware in STM32WL project (https://www.st.com/resource/en/application_note/an4894-eeprom-emulation-techniques-and-software-for-stm32-microcontrollers-stmicroelectronics.pdf) in lieu of writing directly in FLA...
I am following this video link showing step by step to create OTA app.https://www.youtube.com/watch?v=mRzZOa3jmuM.I am successfully to create the custom application, download the OTA loader app at 0x08000000, and the custom's app at 0x08007000. The ...
Hello Geeks...Hope all are doing wellRecently, I'm working on STM32WB FUOTAI know the FUOTA terminology of the STM32WB through the application document AN5247Moreover, I have gone through the YouTube Tutorial series of the FUOTA for WB seriesI'm tryi...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.