2023-03-14 3:40 AM
I'm using a NUCLEO-WB55RG board and if I create a new project in STM32CubeIDE 1.12.0 and enable the STM32_WPAN and HeartRate example it doesn't work because the different buffers that need to be in SRAM2 is not placed there.
The app_entry.c defines these buffers like this:
PLACE_IN_SECTION("MB_MEM2") ALIGN(4) static uint8_t EvtPool[POOL_SIZE];
PLACE_IN_SECTION("MB_MEM2") ALIGN(4) static TL_CmdPacket_t SystemCmdBuffer;
PLACE_IN_SECTION("MB_MEM2") ALIGN(4) static uint8_t SystemSpareEvtBuffer[sizeof(TL_PacketHeader_t) + TL_EVT_HDR_SIZE + 255U];
PLACE_IN_SECTION("MB_MEM2") ALIGN(4) static uint8_t BleSpareEvtBuffer[sizeof(TL_PacketHeader_t) + TL_EVT_HDR_SIZE + 255];The automatically generated linker script contains the following, which ends up placing the buffers in RAM1 if I look at the address at runtime using the debugger.
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 512K
RAM1 (xrw) : ORIGIN = 0x20000008, LENGTH = 0x2FFF8
RAM_SHARED (xrw) : ORIGIN = 0x20030000, LENGTH = 10K
}
<--snipped-->
MB_MEM1 (NOLOAD) : { *(MB_MEM1) } >RAM_SHARED
/* used by the startup to initialize .MB_MEM2 data */
_siMB_MEM2 = LOADADDR(.MB_MEM2);
.MB_MEM2 :
{
_sMB_MEM2 = . ;
*(.MB_MEM2) ;
_eMB_MEM2 = . ;
} >RAM_SHARED AT> FLASHIf I instead create a new project based on the BLE_HeartRate example from "Example Selector", the linker script instead contain:
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 512K
RAM1 (xrw) : ORIGIN = 0x20000008, LENGTH = 0x2FFF8
RAM_SHARED (xrw) : ORIGIN = 0x20030000, LENGTH = 10K
}
<--snipped-->
MB_MEM1 (NOLOAD) : { *(MB_MEM1) } >RAM_SHARED
MB_MEM2 (NOLOAD) : { _sMB_MEM2 = . ; *(MB_MEM2) ; _eMB_MEM2 = . ; } >RAM_SHAREDAnd this works just fine, and the buffers are placed in SRAM2.
I can solve the issue by creating my own section, placing it in RAM_SHARED, or by just editing app_entry.c to place them in MB_RAM1 which is also correctly placed in RAM_SHARED / SRAM2, but if feels like this is a bug that will probably confuse a lot of other people as well.
(My linked script knowledge is a bit limited, so I don't really understand why the auto-generated linker script ends up placing the section in the wrong place.)
Solved! Go to Solution.
2023-03-14 8:53 AM
That makes sense, and if I change it the linker script works as intended. Thanks for pointing it out!
I guess this is a bug in the auto-generated linker script then? Since the code generator generated code that is marked to go into the "MB_MEM2" without the dot, it would make sense if this is what the linker script used as well.
2023-03-14 5:38 AM
> I don't really understand why the auto-generated linker script ends up placing the section in the wrong place
Because in the 1st link script snippet the section name is ".MB_MEM2" (note the dot) but it should be "MB_MEM2" without dot.
2023-03-14 8:53 AM
That makes sense, and if I change it the linker script works as intended. Thanks for pointing it out!
I guess this is a bug in the auto-generated linker script then? Since the code generator generated code that is marked to go into the "MB_MEM2" without the dot, it would make sense if this is what the linker script used as well.
2023-03-24 11:51 AM
Hello,
Thanks for your feedback, indeed there is an extra dot in auto-generated linker script. It will be corrected in the next release.
Best Regards
2023-05-11 4:56 PM
Faced the same issue with STM32WB10CC which was not entering Low-power mode, turns out having this section in wrong place was creating issue with LPM. Changed in a similar fashion as mentioned in STM32WB15CC example and worked afterwards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.