STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4119 Views
  • 0 replies
  • 3 kudos

Resolved! Can't find the schematics of the STM32WB5MM-DK

Edit: It's always embarrassing when you ask a question and immediately afterwards you find what you where looking for...Please ignore this question.---Original question: I'm starting to work with the STM32WB5MM-DK, but I can't find the schematics. Ar...

A.D. by Senior
  • 1771 Views
  • 1 replies
  • 0 kudos

How to set up IEEE 802.15.4 MAC on the STM32WB55RG

I have a question about STM32WB55RGV6. I will list my current progress below.- First of all, I will be using the NUCLEO-WB55RG board to use the IEEE 802.15.4 MAC Stack. ​- I want to communicate with the Xbee S2C (XB24CZ7WIT-004) from Digi to send and...

JLee.19 by Associate II
  • 4856 Views
  • 3 replies
  • 1 kudos

MAC_802_15_4_FFD with other peripherals

I want to use MAC 802_15_4 with other peripherals like SPI2, I2C1 and USB as a CDC device but there is no option in cubemx to generate code for MAC 802_15_4 and i didn't find any application notes to write program for MAC 802_15_4 only i found 2 samp...

DineshB by Associate III
  • 736 Views
  • 0 replies
  • 0 kudos

STM32WL54CCU6 and STM32WLE5CBU6: Receiver Sensitivity Data

Hi,I am evaluating 2 MCUs (STM32WL54CCU6 and STM32WLE5CBU6) for our new design. I would like to get the receiver sensitivity at the following condition: 2-(G)FSK, BER <1%, 200kbps, 50kHz FDA at 915 MHz, which datasheet don't have. When you have a cha...

TNguy.51 by Associate
  • 1634 Views
  • 2 replies
  • 0 kudos

Issues about STM32WB

HiWe develop a project on the STM32WB5MMG MCU. We have 2 issues:1. How can we get the actual MTU after the negotiation with the remote client (probably a smartphone) ? We want to support all kind of smartphones including those with small MTU. Do we h...

Ofer by Senior
  • 2158 Views
  • 4 replies
  • 0 kudos

Resolved! STM32WB5MMG power removed while updating FUS

During testing to see what happens if power is interrupted during various parts of firmware update, I removed power from my test board while updating FUS. Now, when I connect via SWD using STM32CubeProgrammer, it shows the following: When I try to up...

0693W00000bh7sOQAQ.png
crwper by Senior
  • 4476 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.