2023-05-10 9:19 AM - last edited on 2023-11-30 6:54 AM by Amel NASRI
Hi,
I want to choose a ST MCU/MPU and I would like the CPU to have BLE, to be able to run a low power mode (STANDBY), use < 5µA in STANDBY and be able to listen on BLE during STANDBY mode
Best is that BLE chip would be in STANDBY as well but listening
So MCU/MPU + BLE in STANDBY would use less than 50µA
Is there a ST MCU/MPU solution?
Thanks,
2023-05-11 12:21 PM
Look at L4 series with Cortex M4. It's low power consumption MCU 's.
More details here:
https://www.st.com/en/microcontrollers-microprocessors/stm32l4-series.html
2023-05-11 11:17 PM
Thanks Kamil
But these chips does not include BLE, do they?
Best would be a MCU with BLE that can receive RF packets at low power mode and use < 50µA in reception
Is that possible?
Thanks,
2023-05-11 11:27 PM
I forgot about BLE. Look at WB series. It is ultra low power and chip includes BLE:
https://www.st.com/en/microcontrollers-microprocessors/stm32wb-series.html
Check it out:
STM32WB5MMGH6TR
Boards: STEVAL-ASTRA1B - STEVAL-PROTEUS1 - STM32WB5MM-DK
ST declares up to 0,25 uA in Standby mode
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.