NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello all.I am trying to build up a LoRaWAN end node on a single core STM32WLE5. I am new to LoRa development and thought I would leverage the repo LoRaWAN_End_Node which uses the dual core (STM32WL55 Nucleo). I went ahead in the ioc and tried my b...
Hello,we are currently evaluating whether the STM32WB10 is suitable for a new project. Even though the project will not use wireless connectivity, the STM32WB10 is interesting to us because it is used in high volume in another project and is therefor...
STM32 - STM32WB55CGU6 Antenna - 2450AT18B100E Filter - MLPF-WB-01E3 Hello everyone, please help me fix the problem with my custom PCB board and BLE. The antenna on the board won’t work (I don't see my device via Bluetooth) in any way and I don’t...
Our STM32WB55 user application is currently in the HardFault_Handler. (Full disclosure: I am not an embedded developer at all, I have never debugged such a problem, so I'm not really knowing what I am doing. I need precise, detailed step-by-step inst...
Hi, I have STM32WB55.It has 1 UART and 1 low-power Uart (lpuart). And I have SDI12 sensor.I have successfully read whit lpuart SDI12 protocol sensor. But now I want to use ZigBee to send data that I read from the sensor to the Zigbee coordinator. I c...
I'm following this tutorial by the official ST YouTube channel giving a step-by-step guide on sending sensor data to your application server through the network server The Things Network. I have been able to do the tutorial, but I would like to add a...
Hello,Please suggest us, external antennas for STM32WLE5CC for IN865, for longer range coverage.Thank You
I use RAK3172 and I've follow the "RAK3172 on STM32CubeIDE with STM32WL SDK v1.2.0" article, and every things go well with the project named "LoRaWAN_End_Node", except the .ico file is not for STM32WLE5CCU6. How can I change this?
I am trying to implement an HCI interface and the stack is reporting almost nothing supported in the HCI_READ_LOCAL_SUPPORTED_FEATURES command. Why is this? Is there a way to enable the features? I am using stack v1.16. I have tried multiple variatio...
I am trying to follow the "STM32WB Getting started Series: Part 12b lab..."(https://www.youtube.com/watch?v=CKYWy7LKL68&list=PLnMKNibPkDnG9JRe2fbOOpVpWY7E4WbJ-&index=16) on youtube. In the video he is using a WB55, but I am trying to implement it on ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.