STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

How to switch I2C pull up when STOP MODE 2 on STM32WLE

Hello,I have a STM32WLE that works with the lora end_node projectI have a sensor that i power up with a mosfet when needed.But during the time that the chip is sleeping i need to disable the internal I2C pullup (+30 uA more due to the fact that the V...

HDIA.1 by Associate III
  • 1649 Views
  • 1 replies
  • 0 kudos

STM32WL55JC17 LoRaWAN ABP activation problem

Hi, I am using the NUCLEO-STM32WL55JC1 LoRaWAN board, which I have connected to the TTN through the OTAA activation method as seen in the snapshot below. Now I wanna connect it via the ABP activation method, however, the device can't connect to the T...

_legacyfs_online_stmicro_images_0693W00000dDJlxQAG.png _legacyfs_online_stmicro_images_0693W00000dDJnOQAW.png
Junaid.Q by Associate
  • 1100 Views
  • 0 replies
  • 0 kudos

Resolved! About Data transmit with Usart1 using DMA

Hi.I am using STM32WL55.I set USART1 with DMA tx and DMA rx.I tried to transmit some data as follows.  printf("[*] Program Ver 0.2.0.0\r\n");  printf("\r\n");  printf("Net> ");"[*] Program Ver 0.2.0.0\r\n" and "\r\n" are transmitted.but "Net> " is di...

Resolved! How to detect STM32 CubeMX Programmer from my application

I am developing an application on the Seeed Lora-E5 module, which contains an STM32WLE5.Currently I am programming the device via the SWD interface, but for future firmware updates I want to use the UART, (this UART is available externally through a ...

Strooom by Senior
  • 2195 Views
  • 1 replies
  • 3 kudos

BLE HID of STM32WB55 integrated send volume up key

HelloI'm developing a project on chip STM32WB55. I have referenced the demo aboutBLE-HID of ST's "STM32Cube_FW_WB_V1.16.0". The sample code looks define for mouse usage. Could anyone can teach me how to integrated send volume up key into this sample ...

SLin.3 by Associate
  • 900 Views
  • 0 replies
  • 0 kudos

STM32WLE5c general setup.

Hello and good day to you all. I just realised that there were not many articles about the STM32WLE5J in the past and now some topis are added - luckily. And I´m a total beginner to the stm32 enviroment and I really miss a tutorial on how to setup th...

Dodo by Associate II
  • 3024 Views
  • 3 replies
  • 0 kudos

NUCLEO-WB55RG Matter Thread end device commissioning failed

Hello,I am trying to commissioning NUCLEO-WB55RG Matter thread end device. It fails to commission and connect.Reference Source Code used:Matter beta version for STM32 Github repo: github.com/stm32-hotspot/stm32wb-matter-device-over-thread  Setup:1. M...

PKote.2 by Associate II
  • 3935 Views
  • 4 replies
  • 0 kudos

What can prevent entering STOP mode? (STM32WB)

After some activity using BLE in the background and UART as well as some EXTI on application side, the consumption jumps from 2,4µA to 4mA, so obviously I have a wakelock. If I hotplug to the system afterwards, I can see in PWR_EXTSCR that Stop mode ...

OliM by Senior II
  • 3103 Views
  • 0 replies
  • 0 kudos

STM32WB5MMG UART receive interrupt doesn't work

I'm using a STM32WB5MMG chip and I'm trying to receive data with the HAL_UART_Receive_IT() function. But for some reason the HAL_UART_RxCpltCallback function never gets called. Receiving data with blocking mode works, but with an interrupt it doesn't...

Bvan .17 by Associate
  • 1893 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.