2023-06-02 10:30 AM
I am trying to implement an HCI interface and the stack is reporting almost nothing supported in the HCI_READ_LOCAL_SUPPORTED_FEATURES command. Why is this? Is there a way to enable the features? I am using stack v1.16. I have tried multiple variations of the stack.
2023-06-02 11:47 AM
Unfortunately many HCI commands are not supported.
2023-06-02 11:51 AM
Well, the command itself is supported, unfortunately it list most features as not supported, even though I know that they are supported...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.