2022-02-19 8:48 AM
I use the wl55 on the nucleo kit, with the ping pong exemple (one core but same with 2) in subghz_phy_app.h i change the define for
#elif (( USE_MODEM_LORA == 0 ) && ( USE_MODEM_FSK == 1 ))
#define FSK_FDEV 10000 /* Hz */
#define FSK_DATARATE 10000 /* bps */
#define FSK_BANDWIDTH 399000 /* Hz */
#define FSK_PREAMBLE_LENGTH 50 /* Same for Tx and Rx */
#define FSK_FIX_LENGTH_PAYLOAD_ON false
Changing value of FSK_DATARATE don't change data rate on air which stay at about 6800bds (i have try from 50000 to 1000 with the same result)
changing FSK_FDEV change effectivly the spectrum.
i use Gnuradio for these tests.
As far as i can debug trace every thing appear normal, on the subghz SPI 0x8A and 0x8B packet seem correct.
Where and what is the problem ?
JP
2022-02-23 12:37 AM
Hi,
To reformulate my question, has anyone succeeded in changing FSK data rate, on the ping pong example?
I have 2 boards and the example doing very well, but with a wrong data rate.
JP
2022-02-25 6:22 AM
Hi,
I have made a basic test program without the subGHz middleware, and there the data rate can be changed.
So i think the trouble is in the ping pong example.
JP
2023-10-31 2:05 AM
Hello @Xynium
I have just now started with FSk using the B-L072Z LRWAN1 board.
I wanted to know what is the maximum bps/data rate you got using FSK.
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.