STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! [OpenThread] Sending CoAP to Thread SED from leader

I have used the Cube examples "Thread_FTD_Coap_Multicast" and "Thread_SED_Coap_FreeRTOS" and I was able to receive CoAP multicast from SED to the thread leader however I am not able to send messages to the SED in any way at all when I pressed SW1 on ...

Resolved! Use VHF with 2 NUCLEO-WL55JC1

Hello,I bought 2 NUCLEO-WL55JC1 to send and receive some data.I used example code in Lora which work very well (SubGHz_Phy_PingPong).My problem is to use VHF (156.8750Hz).I modify the code (RF_FREQUENCY, FSK_FDEV, FSK_DATARATE, FSK_BANDWIDTH, USE_MOD...

Ted_ by Associate II
  • 2806 Views
  • 4 replies
  • 0 kudos

How to yield a task when sending large amount of data

Hi all,I want to send loads of data to a client whenever it enables notification for that service. What I have now is that I can catch the En/disable of the characteristic notification and start a task on it using the sequencer. However as long as th...

Taxara by Associate III
  • 3360 Views
  • 4 replies
  • 4 kudos

Fast FUOTA only possible when using ST BLE Sensor App

I am trying to implement the OTA feature of the WB55 into my own app. However, the OTA Update is only successful if every packet is exactly 20 Bytes. I tried doing OTA with the BLE Sensor App and that one is much faster, I suppose the App sends somew...

tester by Associate III
  • 2869 Views
  • 2 replies
  • 0 kudos

Question of STM32WB OTA reboot problem

Hello, I have a question about OTA in the stm32wb series.I'm testing to add the OTA function to the board I'm developing.After full erase of MCU, I succeeded in downloading application bin file to MCU with STBLE Toolbox application.Afterwards, to upd...

SKmin by Associate
  • 8666 Views
  • 10 replies
  • 3 kudos

Resolved! STM32WB FOTA Practical Questions

Hi all,Looking to implement FOTA on a custom board which uses the STM32WB55M module. I understand the principles of the FOTA solution and the services/characteristics and have looked over the relevant app note, but I have a couple of questions about ...

TBran.3 by Associate III
  • 16174 Views
  • 19 replies
  • 11 kudos

Resolved! STM32WB HSE tune

Hi,What error on HSE frequency is acceptable by STM32WB35? More than 1 kHz can disturb connection process (its interrupted or it's slow than usual on some phones) or can cause unexpected disconnection? Does this affect the range of the advertisement ...

Resolved! STM32WB Project Application Example missing file

Hello!I am trying to run the BLE_TransparentMode example https://github.com/STMicroelectronics/STM32CubeWB/tree/master/Projects/STM32WB5MM-DK/Applications/BLE/BLE_TransparentMode/STM32CubeIDE I have opened the project in STM32CubeIDE and try to compi...

DLid.1 by Associate II
  • 1371 Views
  • 1 replies
  • 0 kudos

Resolved! What is maximum MSPS for multi-channel ADC?

I need 1.5 MSPS speed for my array device having 1536 pixels. I saw that the STM32WB55VGY6TR microcontroller operates its ADC at a maximum speed of 4.26 MSPS in the manual. So, my question is, if I activate 16 channels (the maximum number of channels...

KKIM.6 by Senior II
  • 3045 Views
  • 1 replies
  • 0 kudos

STM32WL55 FreeRTOS and SubGHz_Phy

Hello everyone,We are a group of students working on the development of flight control and communication software as part of a space program. Our project is based on the STM32Wl55 MCU with LoRa and FreeRTOS. Currently, we are transitioning our softwa...

Bildschirmfoto 2023-10-24 um 16.23.08.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.