STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! Confusion about PA impedance specification of STM32WL31xx

Hi!If I look at the datasheet of STM32WL31xx, I find Table 34. PA impedance which tells e.g. an optimum load impedance of 32 Ω // 16 nH in line 5 (high power, 868MHz) This STM32WL31xx is (according to the datasheet) available in VFQFPN32 and VFQFPN48...

Franz1_0-1767033671854.png
Franz.1 by Associate III
  • 643 Views
  • 3 replies
  • 1 kudos

LoRaWAN End Node DualCore on Linux

Hello, I'm having troubles building the two projects of the STM32 Nucleo WL55JC1 belonging to the LoRaWAN End Node DualCore Example under Linux (Ubuntu 24.04). It works on Windows 11, though.Until now I have all projects developed on Linux, this is m...

bgoedel by Associate II
  • 388 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WL5MOC LSE 32kHz accuracy

Hi,  In the STM32WL5MOC datasheet I can find the 32MHz TXCO HSE accurancy, but not the LSE 32kHz RTC clock accuracy. Could someone look into this and provide the min/max values similar to TXCO characteristics in Table 10? Best Regards,Dave

50_ohm by Associate
  • 339 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WBA52 Standby Mode Example

Hello all,Anyone successfully implemented the Standby Mode for STM32WBA52/55?  I am struggling going thru the examples and I wouldn't be able to enter the standby mode level.  My board still consume about 70mA when I enter the standby mode.  From the...

Resolved! Can't Program or erase NUCLEO-WL55JC1

I have just received 2 NUCLEO-WL55JC1. Upon connecting either one of them via I see The Red (main power) and green LEDs on. The other thre are flashing alternatively (red, orange, blue). I haven't changed the default jumper settings.The following deb...

mapfumo by Associate
  • 529 Views
  • 2 replies
  • 2 kudos

DIMMABLE COLOR LIGHT callbacks never invoked

Hi there and happy new year! I am currently trying to develop a dimmable color light with an stm32wb55 (Nucleo Board). Everything seems to work when connecting the device to a zigbee2mqtt server over zigbee. But actually all color server related call...

Exeu_0-1767261198328.png
Exeu by Associate III
  • 433 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.