2025-12-23 7:48 AM
Hi, team
I previously worked with a SWB (dual core) microcontroller, and I was able to obtain the stack version using the SHCI_GetWirelessFwInfo function. Now, I am working with a SWBA (single core) but I was unable to find an equivalent function to do it. Do you know if there is an equivalent?, I want to know the stack version on compilation time or runtime, it does not matter.
Thanks in advance.
2026-01-05 4:27 AM - edited 2026-01-05 4:27 AM
Hi,
Here is an equivalent function used in the examples of the STM32CubeWBA package (Excerpt from an example of version 1.8.0) :
/* Host Stack Version: 0.15, 0.16... */
uint8_t HCI_Version = 0;
uint16_t HCI_Subversion = 0;
uint8_t LMP_Version = 0;
uint16_t Company_Identifier = 0;
uint16_t LMP_Subversion = 0;
hci_read_local_version_information(&HCI_Version, &HCI_Subversion, &LMP_Version, &Company_Identifier, &LMP_Subversion);
a_GATT_DevInfoData[12] = (uint8_t)((uint16_t)HCI_Subversion & 0xff);
LOG_INFO_APP("-- DEVICE INFO CHAR : Host Stack version = 0x%02X\n", a_GATT_DevInfoData[12]);
/* Host Stack Type: Full, Basic, Basic Plus... */
a_GATT_DevInfoData[13] = (uint8_t)(((uint16_t)HCI_Subversion & 0xff00) >> 8);
LOG_INFO_APP("-- DEVICE INFO CHAR : Host Stack Type = 0x%02X\n", a_GATT_DevInfoData[13]);
Here are the values associated with each host stack.
| Hex Code | Stack Name |
|---|---|
| 0x00 | Full Stack |
| 0x10 | Basic Plus |
| 0x20 | Basic Features |
| 0x40 | Peripheral Only |
| 0x80 | LL Only |
| 0xA0 | LL Only Basic |
BR,
Joé
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.