2026-01-08 3:48 AM
Solved! Go to Solution.
2026-01-08 5:41 AM - edited 2026-01-08 5:50 AM
Welcome @50_ohm, to the community!
I am very sorry that this specification is not mentioned in the data sheet. However, I would like to point out that the frequency accuracy of the 32MHz HSE is an essential prerequisite for proper functioning in some frequency bands.
The built-in LSE crystal has a frequency tolerance of ±20ppm at 25°C and a parabolic coefficient of -0.04ppm/°C². If there are any deviations, you can use the smooth calibration function included in the built-in STM32WL55JC, together with the temperature sensor if necessary. I have also explained the smooth calibration in a more understandable way in this thread. There is also a Knowledge Base article describing the smooth calibration for the STM32U575 which uses a similar RTC.
Hope this answers your question?
Regards
/Peter
2026-01-08 5:41 AM - edited 2026-01-08 5:50 AM
Welcome @50_ohm, to the community!
I am very sorry that this specification is not mentioned in the data sheet. However, I would like to point out that the frequency accuracy of the 32MHz HSE is an essential prerequisite for proper functioning in some frequency bands.
The built-in LSE crystal has a frequency tolerance of ±20ppm at 25°C and a parabolic coefficient of -0.04ppm/°C². If there are any deviations, you can use the smooth calibration function included in the built-in STM32WL55JC, together with the temperature sensor if necessary. I have also explained the smooth calibration in a more understandable way in this thread. There is also a Knowledge Base article describing the smooth calibration for the STM32U575 which uses a similar RTC.
Hope this answers your question?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.