NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
This https://blog.st.com/stm32wl5x-stm32wl5m/ seems to suggest that the wireless module could be either 900 or 800 MHz bands."Hence, coupled with the wide frequency range supported by its STM32WL5x, the module can work in Europe, Americas, and Asia."...
Hi, I am using the NUCLEO-WL55JC1 board and referring to the PWR_STOP2_RTC example to measure current consumption. I have isolated the ST-LINK section and am powering the board with an external 3.6 V supply for accurate measurement. However, in sle...
P-NUCLEO-WB55Just a sanity check really.I'm using the DWT unit to time a chunk of code, am I right that each tick is at 1/32MHz?
Hello. I got my hands on a wba55cg nucleo board and i'm currently studying about ble.I want to create a BLE Beacon that changes its adv_data whenever a user presses one of the button. From messing around using the p2p_server and beacon st examples, i...
I am using LPTIM for pulse counting in ultra low power (stop 2) mode for STM32wl55jc. Now, the problem is on the pin if I connect any pull up/ pull down with 10k-50k range, it draws significant amount of current. Can anyone please suggest a circuit t...
Hello,We are currently working with the NUCLEO-WL55JC1 board for LoRa communication and have a few technical queries. 1. STM32WL as Gateway / P2P ReceiverWe are planning to use two NUCLEO-WL55JC1 boards, where: One board will act as a LoRa end node ...
Hello,Recently, I’ve been asking several questions about STM32WB55 BLE behavior, and the respected @FilipKremen has provided me with great support.It turns out that all this time I was actually working with fake Chinese chips. I suspect that some of...
On a custom board, I would like to use the BlueNRG GUI (v.4.7.1) to run the tests described in AN4818 (rev.8) using the DTM firmware embedded in BlueNRG-1_2 DK 3.2.3.I got a connection and I am able to send basic commands, like ACI_TEST_TONE START an...
Hello ST Community team,About the Typo, on the Table 1 of the RM0473, we have a reserved region between SRAM1 and SRAM2a (from 0x2000 3000 and 0x2002 FFFF) the size of this region is 180 Kbytes and not 36 KBytes as mentioned on the Doc.please have a ...
I am configuring a dual-CPU project for the STM32WL55JC in CubeMX. This microcontroller has two CPUs: a Cortex M4 and a Cortex M0+. CubeMX lets users select the CPU that each peripheral is bound to. As illustrated in the image at the bottom of this p...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.