NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi All, I am wondering, does the STM32WL SubGHz MCU support piggybacking, lik the S2LP radio does?thank you, Arjan
Hi,I would like to use the BLE_p2pServer example with the NUCLEO-WBA52CG board as shown in the MOOC example with the NUCLEO-WBA55CC board. Unfortunately, I can only find this example for the NUCLEO-WBA55CG via the “Example Selector”.Is there a way to...
Hello,I'm using a Nucleo-WB55RE board with Quad SPI in single mode. I'm trying to start very simply by just reading the chip id from a Riverdi BT81X display. I have captured two waveforms, one via a Nucleo-446 board using regular SPI and one from t...
If I comment out "MX_LoRaWAN_Process();" in main, then the USART1 interrupts trigger as they normally would. Could anyone offer some advice of how to add USART1 to the example?Kind regards
Hello all, I am trying to add two virtual COM ports on STM32WB5MMHGx device. The initial code is based out of STM32Cube example: Ux_Device_CDC_ACM. I initially added this piece of code to register the class. cdc_acm_parameter2.ux_slave_clas...
The STM32WL5x Datasheet mentions the RX Sensitivity of the Radio Modem for both 2-FSK and LoRa modulation (see image below) but makes no mention of GFSK, GMSK or BPSKWhat are the receive sensitivity values for these modulation schemes?
I can't seem to get any of the samples to connect using the ST BLE Toolbox or ST BLE Sensor applications. Here's what I have:Uploaded the latest BLE full stack:Uploaded the BLE_HeartRate_reference.hex file:Disconnect/Connected the USB cable to Nucle...
Hey everyone, I am using STM32WB55RGV7 processor. At the beginning of my bootloader programif (((*(__IO uint32_t*)address) & 0x2FFE0000 ) == 0x20000000) // if there is an application at the APP_START_ADDRESS { typedef void(*pFunction)(void);pFunction...
How can a custom BLE mesh be created ?I have already checked all the mesh models provided as example but how can I can make a custom mesh as I need to add a few external sensors.I have checked the MOOC for BLE mesh but it does not tell aything about ...
Hi,I try to build up a HAM LoRa APRS system with STM32 and I don´t receive any messages in my gateway. For testing purposes, I use an 868 MHz gateway and an RAK3172 module. The RAK3172 module is configured as shown below:Initialize the LoRa module (u...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.