2024-09-09 12:11 AM
The STM32WL5x Datasheet mentions the RX Sensitivity of the Radio Modem for both 2-FSK and LoRa modulation (see image below) but makes no mention of GFSK, GMSK or BPSK
What are the receive sensitivity values for these modulation schemes?
Solved! Go to Solution.
2024-09-09 1:59 AM
Hello @MoralkaraLynn and welcome to the ST Community :smiling_face_with_smiling_eyes:.
The sub-GHz radio implemented on the STM32WL5x support Transmission and Reception using the LoRa and the 2-FSK modulations. But it supports only the Transmission for the 2-MSK and BPSK modulation. So, no reception for GMSK, MSK and BPSK. For the GFSK, it is mentioned on the 2-FSK (FSK & GFSK).
Then, RX sensitivity parameter should be available only For LoRa, FSK and GFSK.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-09-09 1:59 AM
Hello @MoralkaraLynn and welcome to the ST Community :smiling_face_with_smiling_eyes:.
The sub-GHz radio implemented on the STM32WL5x support Transmission and Reception using the LoRa and the 2-FSK modulations. But it supports only the Transmission for the 2-MSK and BPSK modulation. So, no reception for GMSK, MSK and BPSK. For the GFSK, it is mentioned on the 2-FSK (FSK & GFSK).
Then, RX sensitivity parameter should be available only For LoRa, FSK and GFSK.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.