2024-08-12 1:43 PM - last edited on 2024-08-16 2:44 AM by Amel NASRI
Hello all,
I am trying to add two virtual COM ports on STM32WB5MMHGx device. The initial code is based out of STM32Cube example: Ux_Device_CDC_ACM.
I initially added this piece of code to register the class.
cdc_acm_parameter2.ux_slave_class_cdc_acm_instance_activate = USBD_CDC_ACM_Activate2;
cdc_acm_parameter2.ux_slave_class_cdc_acm_instance_deactivate = USBD_CDC_ACM_Deactivate2;
cdc_acm_parameter2.ux_slave_class_cdc_acm_parameter_change = USBD_CDC_ACM_ParameterChange2;
uint32_t code;
if ( code = ux_device_stack_class_register("ACM2",
ux_device_class_cdc_acm_entry,
cdc_acm_configuration_number,
cdc_acm_interface_number,
&cdc_acm_parameter2) != UX_SUCCESS )
{
UNUSED(code);
/* USER CODE BEGIN USBX_DEVICE_CDC_ACM_REGISTER_ERORR */
return UX_ERROR;
/* USER CODE END USBX_DEVICE_CDC_ACM_REGISTER_ERORR */
}
Memory pool and USB stack sizes were increased so that this registration process succeds.
That did not show up as two ACM devices on linux. After digging around, I found that there is a bug in the ux_device_descriptors.c.
This piece of code is needed to enumerate and add two classes.
uint8_t UserClassInstance[USBD_MAX_CLASS_INTERFACES] = {
CLASS_TYPE_CDC_ACM,
CLASS_TYPE_CDC_ACM
};
But that does not add proper descriptors and endpoint addresses. I solved this by comparing with NXP device descriptors.
The changes made to get two devices listed as ttyACM1 and ttyACM2 are:
uint8_t USBD_FrameWork_AddToConfDesc(USBD_DevClassHandleTypeDef *pdev, uint8_t Speed,
uint8_t *pCmpstConfDesc)
{
.
.
.
switch (pdev->tclasslist[pdev->classId].ClassType)
{
#if USBD_CDC_ACM_CLASS_ACTIVATED == 1
case CLASS_TYPE_CDC_ACM:
/* Find the first available interface slot and Assign number of interfaces */
interface = USBD_FrameWork_FindFreeIFNbr(pdev);
pdev->tclasslist[pdev->classId].InterfaceType = interface; //! Assign missing interface number.
pdev->tclasslist[pdev->classId].NumIf = 2U;
}
And the address was incremented by InterfaceType.
static void USBD_FrameWork_AssignEp(USBD_DevClassHandleTypeDef *pdev,
uint8_t Add, uint8_t Type, uint32_t Sze)
{
uint32_t idx = 0U;
/* Find the first available endpoint slot */
while (((idx < (pdev->tclasslist[pdev->classId]).NumEps) && \
((pdev->tclasslist[pdev->classId].Eps[idx].is_used) != 0U)))
{
/* Increment the index */
idx++;
}
/* Configure the endpoint */
uint8_t address = Add + pdev->tclasslist[pdev->classId].InterfaceType;
pdev->tclasslist[pdev->classId].Eps[idx].add = address;
pdev->tclasslist[pdev->classId].Eps[idx].type = Type;
pdev->tclasslist[pdev->classId].Eps[idx].size = (uint16_t) Sze;
pdev->tclasslist[pdev->classId].Eps[idx].is_used = 1U;
}
This fixed the issue. Now I see two VCOMs.
[ +0.300216] usb 1-4.3.4: new full-speed USB device number 89 using xhci_hcd
[ +0.190420] usb 1-4.3.4: New USB device found, idVendor=0483, idProduct=5740, bcdDevice= 2.00
[ +0.000005] usb 1-4.3.4: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ +0.000002] usb 1-4.3.4: Product: STM32 Virtual ComPort
[ +0.000002] usb 1-4.3.4: Manufacturer: STMicroelectronics
[ +0.000001] usb 1-4.3.4: SerialNumber: CDC_ACM001
[ +0.016028] cdc_acm 1-4.3.4:1.0: ttyACM1: USB ACM device
[ +0.000428] cdc_acm 1-4.3.4:1.2: ttyACM2: USB ACM device
Also, I added the addresses to the init function:
HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x00 , PCD_SNG_BUF, 0x14);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x80 , PCD_SNG_BUF, 0x54);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x81, PCD_SNG_BUF, 0x94);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x01, PCD_SNG_BUF, 0xD4);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x82, PCD_SNG_BUF, 0x114);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x02 , PCD_SNG_BUF, 0x154);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x82 , PCD_SNG_BUF, 0x194);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x83, PCD_SNG_BUF, 0x1D4);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x03, PCD_SNG_BUF, 0x214);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x84, PCD_SNG_BUF, 0x254);
I am not sure if the above is configuration is correct. I have simply followed the pattern.
Issue:
When two CDC ACM classes are added to device_framework_full_speed, I get gibberish on the COM port.
Simply removing CLASS_TYPE_CDC_ACM from UserClassInstance makes a single COM port and UART work as per the initial example.
I am definitely missing something. Can anyone help me out?
Here is a link to the complete project on GitHub.
Solved! Go to Solution.
2024-09-09 5:35 AM
Hi @FBL ,
Thank you for the response!
Here I have both the ACM's working with USBx stack.
[Sep 9 14:33] usb 1-4.2.1.1: USB disconnect, device number 16
[ +0.185932] usb 1-4.2.1.1: new full-speed USB device number 17 using xhci_hcd
[ +0.090350] usb 1-4.2.1.1: New USB device found, idVendor=0483, idProduct=5710, bcdDevice= 2.00
[ +0.000006] usb 1-4.2.1.1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ +0.000002] usb 1-4.2.1.1: Product: STM32 USB Device
[ +0.000002] usb 1-4.2.1.1: Manufacturer: STMicroelectronics
[ +0.000002] usb 1-4.2.1.1: SerialNumber: 000000000001
[ +5.275823] cdc_acm 1-4.2.1.1:1.0: ttyACM0: USB ACM device
[ +0.717204] cdc_acm 1-4.2.1.1:1.2: ttyACM2: USB ACM device
2024-08-13 3:49 AM
Bus 001 Device 032: ID 0483:5740 STMicroelectronics Virtual COM Port
Device Descriptor:
bLength 18
bDescriptorType 1
bcdUSB 2.00
bDeviceClass 239 Miscellaneous Device
bDeviceSubClass 2 [unknown]
bDeviceProtocol 1 Interface Association
bMaxPacketSize0 64
idVendor 0x0483 STMicroelectronics
idProduct 0x5740 Virtual COM Port
bcdDevice 2.00
iManufacturer 1 STMicroelectronics
iProduct 2 STM32 Virtual ComPort
iSerial 3 CDC_ACM001
bNumConfigurations 1
Configuration Descriptor:
bLength 9
bDescriptorType 2
wTotalLength 0x008d
bNumInterfaces 4
bConfigurationValue 1
iConfiguration 0
bmAttributes 0xc0
Self Powered
MaxPower 50mA
Interface Association:
bLength 8
bDescriptorType 11
bFirstInterface 0
bInterfaceCount 2
bFunctionClass 2 Communications
bFunctionSubClass 2 Abstract (modem)
bFunctionProtocol 1 AT-commands (v.25ter)
iFunction 0
Interface Descriptor:
bLength 9
bDescriptorType 4
bInterfaceNumber 0
bAlternateSetting 0
bNumEndpoints 1
bInterfaceClass 2 Communications
bInterfaceSubClass 2 Abstract (modem)
bInterfaceProtocol 1 AT-commands (v.25ter)
iInterface 0
CDC Header:
bcdCDC 1.10
CDC Call Management:
bmCapabilities 0x00
bDataInterface 1
CDC ACM:
bmCapabilities 0x02
line coding and serial state
CDC Union:
bMasterInterface 0
bSlaveInterface 1
Endpoint Descriptor:
bLength 7
bDescriptorType 5
bEndpointAddress 0x82 EP 2 IN
bmAttributes 3
Transfer Type Interrupt
Synch Type None
Usage Type Data
wMaxPacketSize 0x0008 1x 8 bytes
bInterval 5
Interface Descriptor:
bLength 9
bDescriptorType 4
bInterfaceNumber 1
bAlternateSetting 0
bNumEndpoints 2
bInterfaceClass 10 CDC Data
bInterfaceSubClass 0 [unknown]
bInterfaceProtocol 0
iInterface 0
Endpoint Descriptor:
bLength 7
bDescriptorType 5
bEndpointAddress 0x01 EP 1 OUT
bmAttributes 2
Transfer Type Bulk
Synch Type None
Usage Type Data
wMaxPacketSize 0x0040 1x 64 bytes
bInterval 0
Endpoint Descriptor:
bLength 7
bDescriptorType 5
bEndpointAddress 0x81 EP 1 IN
bmAttributes 2
Transfer Type Bulk
Synch Type None
Usage Type Data
wMaxPacketSize 0x0040 1x 64 bytes
bInterval 0
Interface Association:
bLength 8
bDescriptorType 11
bFirstInterface 2
bInterfaceCount 2
bFunctionClass 2 Communications
bFunctionSubClass 2 Abstract (modem)
bFunctionProtocol 1 AT-commands (v.25ter)
iFunction 0
Interface Descriptor:
bLength 9
bDescriptorType 4
bInterfaceNumber 2
bAlternateSetting 0
bNumEndpoints 1
bInterfaceClass 2 Communications
bInterfaceSubClass 2 Abstract (modem)
bInterfaceProtocol 1 AT-commands (v.25ter)
iInterface 0
CDC Header:
bcdCDC 1.10
CDC Call Management:
bmCapabilities 0x00
bDataInterface 3
CDC ACM:
bmCapabilities 0x02
line coding and serial state
CDC Union:
bMasterInterface 2
bSlaveInterface 3
Endpoint Descriptor:
bLength 7
bDescriptorType 5
bEndpointAddress 0x84 EP 4 IN
bmAttributes 3
Transfer Type Interrupt
Synch Type None
Usage Type Data
wMaxPacketSize 0x0008 1x 8 bytes
bInterval 5
Interface Descriptor:
bLength 9
bDescriptorType 4
bInterfaceNumber 3
bAlternateSetting 0
bNumEndpoints 2
bInterfaceClass 10 CDC Data
bInterfaceSubClass 0 [unknown]
bInterfaceProtocol 0
iInterface 0
Endpoint Descriptor:
bLength 7
bDescriptorType 5
bEndpointAddress 0x03 EP 3 OUT
bmAttributes 2
Transfer Type Bulk
Synch Type None
Usage Type Data
wMaxPacketSize 0x0040 1x 64 bytes
bInterval 0
Endpoint Descriptor:
bLength 7
bDescriptorType 5
bEndpointAddress 0x83 EP 3 IN
bmAttributes 2
Transfer Type Bulk
Synch Type None
Usage Type Data
wMaxPacketSize 0x0040 1x 64 bytes
bInterval 0
Device Status: 0x0001
Self PoweredHere is the configuration extracted from lsusb.
`lsusb -d 0483:5740 -v`
I have also modified the config to match the endpoint address.
VOID USBX_APP_Device_Init(VOID)
{
/* USER CODE BEGIN USB_Device_Init_PreTreatment_0 */
/* USER CODE END USB_Device_Init_PreTreatment_0 */
/* USB_FS init function */
/* Enable USB power */
HAL_PWREx_EnableVddUSB(); MX_USB_PCD_Init();
/* USER CODE BEGIN USB_Device_Init_PreTreatment_1 */
/* USER CODE BEGIN EndPoint_Configuration */
HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x00 , PCD_SNG_BUF, 0x14);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x80 , PCD_SNG_BUF, 0x54);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x81, PCD_SNG_BUF, 0x94);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x01, PCD_SNG_BUF, 0xD4);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x82, PCD_SNG_BUF, 0x114);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x02 , PCD_SNG_BUF, 0x154);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x83, PCD_SNG_BUF, 0x194);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x03, PCD_SNG_BUF, 0x1D4);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS, 0x84, PCD_SNG_BUF, 0x214);
/* USER CODE END EndPoint_Configuration */
/* USER CODE END USB_Device_Init_PreTreatment_1 */
/* Initialize and link controller HAL driver */
ux_dcd_stm32_initialize((ULONG)USB, (ULONG)&hpcd_USB_FS);
/* Start the USB device */
HAL_PCD_Start(&hpcd_USB_FS);
/* USER CODE BEGIN USB_Device_Init_PostTreatment */
/* USER CODE END USB_Device_Init_PostTreatment */
}
2024-09-06 9:14 AM
Hi @NRedd.2
You can get inspired with the example provided here How to implement a dual CDC ACM USB device using t... - STMicroelectronics Community though it uses ST library.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-09-09 5:35 AM
Hi @FBL ,
Thank you for the response!
Here I have both the ACM's working with USBx stack.
[Sep 9 14:33] usb 1-4.2.1.1: USB disconnect, device number 16
[ +0.185932] usb 1-4.2.1.1: new full-speed USB device number 17 using xhci_hcd
[ +0.090350] usb 1-4.2.1.1: New USB device found, idVendor=0483, idProduct=5710, bcdDevice= 2.00
[ +0.000006] usb 1-4.2.1.1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ +0.000002] usb 1-4.2.1.1: Product: STM32 USB Device
[ +0.000002] usb 1-4.2.1.1: Manufacturer: STMicroelectronics
[ +0.000002] usb 1-4.2.1.1: SerialNumber: 000000000001
[ +5.275823] cdc_acm 1-4.2.1.1:1.0: ttyACM0: USB ACM device
[ +0.717204] cdc_acm 1-4.2.1.1:1.2: ttyACM2: USB ACM device
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.