STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32WL55 DEBUG MODE ISSUE

Hello,I have a project on STM32WL55 which runs on dual core CM0+ and CM4.When i put it in debug mode using the development board STM32WL55 Nuleo-64 (NUCLEO-WL55JC1), it goes into debug mode without any issue. Both the cores are getting debugged.Proce...

Somya by Associate II
  • 282 Views
  • 2 replies
  • 0 kudos

Resolved! No advertisments from NUCLEO-WB55RG

HiI recently received a NUCLEO-WB55RG (the big board, not the USB dongle) and tried installing the demo from the STM32CubeWB repository.I saw that I need to flash the FUS + Stack first which I did. STM32CubeProg reports FUS State: FUS_IDLEFUS Status:...

Thomas L. by Associate III
  • 276 Views
  • 2 replies
  • 0 kudos

STM32WLxx: LoRaWAN FW 1.4 and AES accelerator

It appears that the STM32WLxx FW 1.4 package includes a LoRaWAN stack that implements AES in software. Is there a technical reason that the AES accelerator in the STM32WLxx is not used? I can imagine things like:AES hardware functionally uses more po...

The project in this link is encountering compilation errors

利用Opus在STM32WB上实现BLE全双工语音流 | 新闻中心 | STM32/STM8 | MCU单片机 | 意法半导体STM | STMCU中文官网   The project in this link is encountering compilation errors.   *This post has been translated from Chinese to comply with the ST Community guidelines.

Resolved! BLE Periodic Advertisement with Response on STM32WBA

Hi, I know that currently STM32WB0 is the only family of BLE MCU that currently supports BLE PAwR, but this MCU is very limited in terms of on-board peripherals, RAM and other features. The STM32WBA series looks like a promising candidate for one of ...

MManj.1 by Associate II
  • 314 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.