STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32WB05TZ fails MX_RTC_Init()

I have a problem with the RTC initialization on the STM32WB05TZF6TR (BGA package).  When the board is powered on, the MX_RTC_Init() function calls HAL_RTC_Init(), which returns with HAL_ERROR status.I traced the problem to the stm32wb0x_hal_rtc.c fil...

DG_NC by Associate II
  • 558 Views
  • 6 replies
  • 0 kudos

Best Mcu for live video recording

Hey guys I am currently looking for an mcu to get started developing a live stream camera board which should be in 7x80 mm dimensions what mcu should I get ? I think 5x5 footprint should be ok but not sure 6x6 also be ok. I am open any advice also ne...

Emircan by Associate
  • 391 Views
  • 4 replies
  • 2 kudos

Resolved! X-NUCLEO-GFX01M2 on WB55RG only gives blank LCD

I am trying to bring up the GFX01M2 on a WB55RG board. Following any of the Custom, FlashLoader, or HelloWorld applications (from the X-CUBE-DISPLAY_3-0-0 download) using STM32CubeIDE merely results in a blank LCD. I feel I'm missing something simple...

DavePfz by Associate III
  • 380 Views
  • 4 replies
  • 2 kudos

PNUCLEO LRWAN3 Connection Issue

Dear ST Support Team,I am currently working on verifying a LoRaWAN proof of concept using STM32 hardware.My setup consists of a LoRaWAN end node and a gateway connected to the Loriot network server. From the Loriot dashboard, I can confirm that the g...

Premauda by Associate
  • 234 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WBA64CIUx USART BOOTLOADER

Hi, I have a problem with activating USART bootloader. I use USART1. Please for details about how to going in bootloader mode. Pattern 12 in  AN2606 is super complicated for me. I use now boot pin. I put it to GND and power ON . By me MCU going in bo...

Brussl by Associate III
  • 755 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.