NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi all,I’m working on an STM32WB55 and trying to run two advertisements “in parallel”:a connectable advertisement (for normal connections / data)a non-connectable advertisement using Additional BeaconI can see both advertisements from an Android devi...
Code is written using stm32CubeMX. Connecting with stmlink V3 Minie. Executing step by step, it appears that debug fails (lose connection) when executing debug_init. In fact debug_init creates the problem when programming pa13.When removing the initi...
Hi STM32 experts, I've been digging through the STM32WBA65RI datasheet and the RM0515 STM32WBA6xxx advanced Arm®-based 32 MCUs but can't seem to locate the factory default values for the FLASH_OPTR register for the STM32WBA65. Unliked the solution fr...
In AN2606 Rev 69, the STM32WBA6x system bootloader section describes the UART interface as USART3, but there appear to be errors:1. Inconsistency within the same entry:The TX pin description mixes USART2 and USART3 in the same sentence:USART3_TX pin ...
Starting with the BLE_Heartrate example, I want to measure a voltage on PA8 of STM32WBA65. The BLE_Heartrate project already has the option of using ADCCTRL to read the internal temperature so as to calibrate the BLE power.I have added PA8 as ADC_Cha...
Hi everyone, I am working with the STM32-NUCLEO-WL55JC2 board and I want to transmit ADC values over LoRa radio. Since this is a dual-core MCU (Cortex-M4 + Cortex-M0+), I would like to clarify the recommended implementation approach. My goal is: Rea...
Hello all :)I am designing a board using the STM32WL33CCV6TR, and want to program/debug using the SWD interface. However, there are multiple pins the SWDIO and SWCLK can be mapped to using alternate functions. Usually with STM products, I have seen a...
Hi,I'm using a Nucleo stm32WL55JC1 board, and i'm trying to run the SBSFU_2_Slots_DualCore example. Used the example selector to start the project. When I tried to compile any of the sub projects they all fail and i have a lot of warnings for include...
Hi,I am trying to make a basic Enhanced Advertising low power application using Arduino IDE.I use a standard P-NUCLEO WB55.I need Arduino IDE because this application is intended to be open for modifications.The current STM Documentation (https://wik...
Greetings,in one of my current projects i am using a STM32WB55 as peripheral which requests a secure connection with the host (bonding mode = 1). When the connection is newly established, everything works as expected - the "pairing" dialogue pops up ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.