cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WLxx: LoRaWAN FW 1.4 and AES accelerator

Dana Myers
Senior

It appears that the STM32WLxx FW 1.4 package includes a LoRaWAN stack that implements AES in software. Is there a technical reason that the AES accelerator in the STM32WLxx is not used? 

I can imagine things like:

  • AES hardware functionally uses more power, or increases latency waking from STOP2, than the Semtech implementation.
  • AES hardware does not provide the functionality required by LoRaWAN (at first glance, this does not appear to be the case).
  • It's just too organizationally difficult to fork the Semtech code to use the AES hardware, or there is some licensing wrinkle (I can't imagine such a thing).

If there's no reason not to use the AES hardware, I'd like to explore doing so.

0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.