NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I'm executing the P2P Server on an STM32WB. I have a custom client that can be ported to different platforms. When I build the client for Windows-11, message exchanges greater than 20 bytes work okay. When I build and run on Android, the P2P respo...
Hy, we struggle to get P-L496G-CELL02 up and running. We created a Cube IDE Software project and are able to send AT commands to BG96. Now we entered a plastic SIM from 1nce and try to connect. Unfortunately we can not select plastic SIM. There is a ...
Hello everyone, do ST actually plan to support STN (Time Sensitive Networking) on their wireless products ? For industrial applications this would probably be an interesting alternative to Profibus if it is robust enough :) Greetings,Andreas
I would like to know percentage of memory usage of the ROM and the RAM of the microcontroller from output file.note ** I use source from application example named BLE_p2pClient under the Projects directory of the STM32Cube_FW_WB_V1.2.0 FW pacakge.
My STM32WB55 is configured as I2C master and connected to an I2C slave.My I2C block is configured like this:I2C->CR1 = 0x01I2C->CR2 = 0x000A0060 (slave address=0x60 and NBYTES=0x0A)To start the I2C transaction I2C->CR2.START is set to 1.I2C communica...
Hi,Today I received a new board from a distributor and used the Hands-On_WS_WBA55 example for initial tests. Everything worked fine. A few hours later, I reconnected the board to the USB board and wanted to flash the firmware. Since then I get the er...
I am trying to debug a sample project from st website and but it is stuck in the first line of main (assembly ) meanwhile when I flash the .hex with cube programmer , the project works perfectly. So I assume that it's a problem with the debugger.I ma...
Hello,How to use ST link programmer from NUCLEO-WB55RG to connected to STM32WB5MMG module to flash my code.
Hello, Is there a PDF describing - how to move code for NUCLEO-WB55RG to STM32WB5MMG module ?
Hi,I'm having an issue regarding sending commands to the Bootloader by UART. My commands are followed by a NACK. I'm working with an STM32WL5MOC and my baudrate is set at 9600 (Also tried with 115200). Here's my sequence:Sending 0x7F twice and receiv...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.