STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Lora transmission with NUCLEO-L073RZ

Hi,I am trying to get the LoRaWAN test project running using the Nucleo-L073RZ and I-NUCLEO-LRWAN1. However, the official STM example does not transmit. Can you help me figure out the issue?

kifsha by Associate II
  • 5531 Views
  • 11 replies
  • 0 kudos

Resolved! STM32WBA52CG BLE not working

I am evaluating the BLE feature of STM32WBA52CG with the NUCLEO-WBA52CG board.I followed the following wiki page and successfully built and flashed the example code.https://wiki.st.com/stm32mcu/wiki/Connectivity:STM32WBA_BLE_STM32CubeMX Here is the l...

ee1234 by Associate II
  • 3590 Views
  • 5 replies
  • 1 kudos

Resolved! STM32WB55CG Zigbee connection with Custom Project

Hi,I am still trying to intetrage my custom board with an STM32WB55CG into my Tuya/Smartlife System with the target of transmitting sensordata and receiving commands (e.g. LED color).In this https://community.st.com/t5/stm32-mcus-wireless/stm32wb55cg...

vh789 by Associate III
  • 1899 Views
  • 3 replies
  • 1 kudos

Resolved! BLE OTA software options

According to AN5247 I can use ST BLE Sensor to perform a BLE OTA firmware update. I've added the reboot characteristic to my design, but how can I get ST BLE Sensor to recognize my custom board? There appears to be an option to add a new design, but ...

signal-2024-09-22-20-50-44-809.jpg
Jcoll.1 by Associate III
  • 1448 Views
  • 1 replies
  • 2 kudos

Resolved! Porting the Ble_ota example

I have a board based on the same chip as the ble_ota example. When I try to run this code on my board I'm finding that it immediately crashes. The crash happens before the debugger even hits the first line. I'm assuming this is something simple, mayb...

Jcoll.1 by Associate III
  • 2335 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.