NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Device STM32WLE5 Clock configuration SYSCLK : MSI 16 MHz (MSIPLL mode Enabled)LSE : 32.768 kHz crystalLPTIM2 kernel clock : LSELow power mode : Sleep Observed behavior When configuring LPTIM2 with LSE clock, the following code sometimes blocks be...
Hi, I'm using an STM32WL5MOC where the LPUART is used to wake up the module from Stop2 mode. Since I have a lot of data to transfer, I would like to ask how I can switch to the HSI clock after waking up, and then, of course, switch back to the LSE to...
Hello.I'm currently working on the above cpu and trying to implement a custom ble p2p server app. I have 1 service and 2-3 characteristics and i want to add Freertos for time critical constraints managenments. Correct me if im wrong, but it seems tha...
Issue Description:I am using the `STM32_Programmer_CLI` to flash the BLE Wireless Stack on an STM32WB series MCU. However, after the programming process is complete, the memory read returns an unexpected value at the Stack Version address, even thoug...
I have come across an issue which I believe is a bug in the implementation of the osThreadFlagsWait function. Scenario A thread is waiting on a flag (e.g. 0x2u) for a timeout above 0, before this timeout should occur, there are multiple other flags s...
Hello everyone, as mentioned in the title, I'm using STM32WBA in a project. Immediately after sending data to the stm32wba coordinator, I add an expression to the backup register and reset the processor using `Nvic_system_reset`. I check this at s...
Are there any expansion boards with Quad SPI NOR Flash chips? I am interested in using it with a NUCLEO-WB55RG board.Preferably it should use the Macronix 25L6433FM2I-08G chip, but that is not a hard requirement. This chip is found on the X-NUCLEO-GF...
Is there any way to optimize the IPD BALFHB-WL-01D3 to work at 865MHz at 22dbm for STM32WL55? And is there any hardware design guide for power of STM32WL like it is there Hardware design guide for STM32L0 application note AN4467.
Hi ST Community,I’m working with STM32WBA (STM32WPAN / BlueNRG-style stack APIs). I’m using Extended Advertising on the peripheral (connectable + scannable, secondary PHY = Coded) and a STM32WBA central that scans and then calls aci_gap_create_conne...
Hello everyone, this is my first time using an ST microcontroller. Specifically, I am using the MB1389E (NUCLEO-WL55JC1) development board. It has been a bit confusing because most of the tutorials have an old version of STM32CubeIDE where everything...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.