2026-03-04 10:42 PM - last edited on 2026-03-05 10:49 AM by Andrew Neil
Hello,
I am using NUCLEO-WB05KN1 development board with the embedded STM32WB05KN MCU.
My goal is to advertise in Eddystone UID frame format.
Currently I generate the advertising packet manually and insert:
10-byte Namespace ID
6-byte Instance ID
Advertising works correctly.
I want to be able to change:
Namespace ID
Instance ID
remotely from a mobile phone using nRF Connect (by writing to a custom GATT characteristic).
This is important because we will deploy many devices in the field and updating IDs over BLE would be very useful.
I created a custom GATT service with two writable characteristics:
aci_gatt_srv_attribute_modified_event()
I handle write events using:
When I receive new data:
I update Namespace_ID / Instance_ID
Then I restart advertising after disconnection
Advertising packet is generated using:
Prepare_Eddystone_UID_Adv_Data()Even though the characteristic write event works and my arrays are updated, the advertising data does NOT seem to change properly after restart.
Questions:
Is it officially supported to dynamically change Eddystone UID fields during runtime?
Do I need to call aci_gap_set_advertising_data() again explicitly after modifying the arrays?
Is there any limitation in STM32WB05 stack regarding advertising data update while connected?
Is stopping advertising → updating data → restarting the correct approach?
Is there any ST example demonstrating dynamic advertising data update?
After writing new Namespace/Instance ID via GATT:
Device disconnects
Advertising restarts
New advertising packet contains updated UID
Any guidance or reference example would be greatly appreciated.
Thank you.
Solved! Go to Solution.
2026-03-19 2:48 AM
Hello @burak_Guzeller,
to your questions:
1) Yes, advertising data can be changed dynamically.
2) Yes, you have to. Updating your local arrays is not sufficient
3) No, there is not, since when the device is connected, it cannot advertise
4) Yes, as it is said in Bluetooth® Low Energy stack v4.x programming guidelines:
The content of the buffer containing the advertising/scan response data is directly accessed by the stack, hence it
should not change when device is advertising.
5) I am not aware of any example where the adv data would change, but you can refer to the programming guidelines above or to Introduction to the STM32WB0 Bluetooth® LE wireless interface
Hope this helps
Best regards
grohmano
2026-03-05 10:02 PM
This is urgent, can you please help? @Tesla DeLorean @grohmano @Aziz BRIGUI
2026-03-19 2:48 AM
Hello @burak_Guzeller,
to your questions:
1) Yes, advertising data can be changed dynamically.
2) Yes, you have to. Updating your local arrays is not sufficient
3) No, there is not, since when the device is connected, it cannot advertise
4) Yes, as it is said in Bluetooth® Low Energy stack v4.x programming guidelines:
The content of the buffer containing the advertising/scan response data is directly accessed by the stack, hence it
should not change when device is advertising.
5) I am not aware of any example where the adv data would change, but you can refer to the programming guidelines above or to Introduction to the STM32WB0 Bluetooth® LE wireless interface
Hope this helps
Best regards
grohmano
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.