STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! Cannot Compile When using example ioc

Hello, first time poster.I recently got a few NUCLEO-WL55JC2's for a research project.but other than the standard examples, I am unable to compile a project that I either made using my own ioc, or the one in C:\Users\%username%\STM32Cube\Repository\S...

TheNeg0t1ator_0-1740148366084.png

Resolved! Secure Flash Area Modification on STM32WB15CC ?

I am using the STM32WB15CC and encountered an issue when my program exceeded 112KB (0x1C000), causing the flashing process to fail. I noticed that the memory region starting from 0x0801C000 is set as a secure flash area.I would like to know if it is ...

hanyang by Associate II
  • 1025 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WB15CC (B-WB1M-WPAN) cannot initilize MotionFx

I've been using B-WB1M-WPAN board with a modified example of motion service from BLE_HR_p2p_Sensor. but with IMU readings with a steval-mki217v1 shield connected with SPI. I already have the CRC checked from CubeMX generation.   So far I have been ab...

Zefie by Associate II
  • 2165 Views
  • 2 replies
  • 0 kudos

Resolved! STM32WB05KZ POWER ANTENNA modification

Hello    For the Nucleo STM32WB05KZ board, the transmission power is normally 0 dBm by default (it can go up to 8 dBm). Is it possible to modify the transmission power according to my needs, for example to 3 or 4 dBm, using STM32CubeProgrammer or ano...

ljm by Associate III
  • 3611 Views
  • 10 replies
  • 0 kudos

Resolved! STM32WLE4 details incorrect - no LoRa?

On this page: https://www.st.com/en/microcontrollers-microprocessors/stm32wle4c8.htmlThe device is specified as having LoRa support in the first paragraph of the description but lower down in the "More from the product line" section the WLE4 chips ar...

robdobsn by Associate
  • 1420 Views
  • 3 replies
  • 2 kudos

Resolved! Unable To Activate PLL64M on STM32WB05TZ/BlueNRG-LPS

I'm building an application for a BlueNRG-LPS (332), now rebranded as STM32WB05TZ (WLCSP-36 Package) by starting with a simply Blinky project testing the clock signals of my device. I need to enable the PLL64M clock source to use the radio peripheral...

DCMilla_3-1725992152306.png DCMilla_1-1725990045903.png DCMilla_0-1725989851102.png DCMilla_2-1725990496445.png
DCMilla by Associate II
  • 3459 Views
  • 8 replies
  • 0 kudos

Resolved! Zigbee Broadcast communication

Hello,I'm working on a project started from Zigbee_APS_coord and Zigbee_APS_router examples on NUCLEO-WB55.USBDongle with STM32Cube_FW_WB_V1.21.0.The project is based on data exchange between the coordinator and several devices acting as routers (fro...

tcpctrnk by Associate III
  • 2125 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.