2025-02-13 7:36 AM
Hi,
i am using STM32WBA55 with BLE_p2pServer_ota example and want to wake-up over an USART2 event (start bit or rising edge) from stop mode. What is a good way to do this? I am using HSI16 with USART2 GPDMA1.
2025-02-13 8:25 AM
Hello @ledi7
You can use some of the USART2 interrupts to wake up the STM32WBA55 from STOP mode. To do that, you need to configure one of the interrupts that wake up from this low power mode. More details are available on the RM0493 parts 39.6 and 39.7.
Best regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-02-15 2:06 AM
Hello @STTwo-32 ,
Thanks for the advice, but what I really want to know is what is the best way to wake up from stop mode by an event on the USART2 interface (Rx pin PA11) to process the USART-Rx data.
Is it good to do the following steps?
1. init PA11 as GPIO_EXTI11 with rising edge
2. as soon as a rising edge on PA11 triggers the interrupt -> Init USART2 and receive Rx data.
3. as soon all data are received -> Init PA11 as GPIO_EXTI11 with rising edge and de-init USART2
4. enter stop mode
Or are there other, better options, e.g. USART2-Rx wake-up with start bit?
2025-03-21 5:36 AM
Hello @STTwo-32 ,
I have studied the user manual RM0493, parts 39.6 and 39.7, but I can't figure out exactly what I need to do. Can you maybe give me a code example? I need to wake up in STOP mode with GPDMA to receive some bytes over USART2.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.