NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I attempting to run the dual core ping pong example.When I attempt to load the program to the CM0+ core I receive the following error message: STMicroelectronics ST-LINK GDB server. Version 7.9.0 Copyright (c) 2024, STMicroelectronics. All rights res...
Sono partito dall'esempio BLE personalizzato per il core WB55RG, che esegue regolarmente Advertising. Tuttavia, ora vorrei aggiungere una scan_request (sto cercando di replicare l'esempio P2P_router partendo da un esempio BLE_custom per avere servizi...
Hey everybody,I am currently working on a project which involves a firmware update over the air (using the nucleo wl55jc1 board). i have found an example project through the official website (https://www.st.com/en/embedded-software/stm32cubewl.html) ...
HiI've tried to build the three FUOTA projects. Each one fails with similar errors. "Missing files".I have a fresh install of the CubeIDE, and I've tried this on two different computers.For example, I built the Single Core FUOTA example for the Nucle...
Hi, I tried to setup BLE, I do not know how I managed first time to success - but I can't do it anymore :DOnce it was working and even tried to send characters, but now I cant setup it anymore.I follow up https://wiki.stmicroelectronics.cn/stm32mcu/w...
Hi, I am testing ble audio with STM32WBA55G-DK1 board. I develop my ble audio application with tmap profile. I referred to BLE_Audio_TMAP_Periopheral project provided by ST. It can be paired and enable le audio. But when i play the music on the an...
Hello everyoneWe are developing a prototype of vibration monitor system . Now we are in optimization stage , reducing the power of the device . We are using SeedStudio Lora E5 HF (STM32WE5) (US915) https://files.seeedstudio.com/products/317990687/res...
Hi,I'm using STM32WB5MMG and placed it in the top left corner of the PCB as recommended. The component assembly is top side only so I can't place the decoupling capacitors for VDD, VDDA, VREF+. Also, the schematic of Sparkfun's MicroMod Processor usi...
Hello,We have a project that uses STM32WB55 as the main controller.This project has certain requirements for power consumption and wants to enter sleep mode through stop2 mode.But I tested the power consumption current of stop2 mode on the STM32WB55 ...
Hi community, I understand that users can encrypt and sign firmware using STM32CubeProgrammer. My question is about the first stage bootloader provided by ST. From my limited reading, it seemed that this 1st stage ST bootloader is only encrypted but ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.