2024-12-11 6:42 AM
Hey everybody,
I am currently working on a project which involves a firmware update over the air (using the nucleo wl55jc1 board). i have found an example project through the official website (https://www.st.com/en/embedded-software/stm32cubewl.html) and unzipped the file directly onto my c disk and use powershell to execute the scripts. at first i tried the code without changes besides the changes in the se-identity.h file and everything worked fine see the picture below for the ouptut on the serial monitor.
working_classA
once i concluded the project worked i tried to change the class from A to C and got the following
i expected to still see the tx sending data. however that just stopped. i did a deep dive into the code but that just got me more confused. its getting me nowhere and i am not sure on how to proceed. i hope you fine people may shine some light on it. i am using chirpstack as networkserver.
2025-01-07 3:24 AM
Hello @IdiotStudent
It may be an issue on the gateway side. Are you sure is not that?
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-24 4:18 AM
Hii,
I also made the same changes and flashed the end node but my program gets stuck on KMS_init function
Could you provide some guidance on this ?
Reagrds,
Suyash
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.