2022-02-17 2:26 AM
Hi,
I want to do something like this:
1) receive button input from touchGFX
2) execute operations to be processed
3) switch to the previous screen or a specific screen.
I run it as below, but the same screen appears.
void bookScreenOperView::operOKFunction()
{
//report to presenter and update text
presenter->userSetOperOK();
bookScreenOperView::tearDownScreen();
}
How can I solve this problem ?
Best regards,
2022-02-17 3:08 AM
Hi,
You can use touchgfx designer.Add a button,and then select "Change screen" for your expected screen.
If you want to do something between click button and change screen ,you should add new interaction which choose to execute C++ code.Remember to tick the box.And then add new interaction which use another interaction is done trigger to change screen.
2022-02-17 10:41 AM
Hello Hwoo-,
Zwei.9,'s answer looks pretty good, this is how we change screens with buttons. For more details, I invite you to follow this tutorial, it will show you how to implement that step by step.
/Osman
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.