STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! How to use TouchGFX designer with STM32CubeIDE

Problem Occurrence Process : Create STM32H747-DISCO Project with TouchGFX Designer -> rename Screen1 of TouchGFX Designer to Main -> rename project files in Windows folder window -> Build in STM32CubeIDE -> Run (error occurred)​I proceeded in the sam...

Does anyone know how this error can be solved? Error: Cannot find the specified linker script. Check the linker settings in the build configuration.

Good morning, kind colleagues. I am working on a project with the STM32F746G-DICO board in the STM32Cube IDE 1.5.1 development environment and the TouchGFX 4.16.0 graphics generator.But when compiling the project there are 3 errors.1. Error: cannot f...

JSarm.1 by Associate
  • 6934 Views
  • 5 replies
  • 0 kudos

How to change to the previous screen

Hi,I want to do something like this:1) receive button input from touchGFX2) execute operations to be processed3) switch to the previous screen or a specific screen.​​I run it as below, but the same screen appears.void bookScreenOperView::operOKFuncti...

Hwoo- by Associate II
  • 2004 Views
  • 2 replies
  • 0 kudos

Popup with return value

Hi,I'd like to have a popup in my app, in which the user can press "Confirm" or "Cancel".I'm looking for a way to have my code written like this:popup_res = show_popup(); if(popup_res == true){ /* user clicked on 'confirm'. do something */ } else...

CHech.1 by Associate III
  • 2228 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.