2024-02-04 10:22 AM
Hello.
I have a SwipeContainer and it works very well.
I put a lot of elements in swipeContainer and I don't have low fps. But if I put dynamic graphics and add data to the graphics, the fps drops a lot.I realize that drawing graphics is very computationally demanding.
I wonder if there is anything I can do to improve performance
Thanks
2024-02-06 5:28 AM
Hello @snnzdmr1 ,
Are you using one graph inside your container? Or are you using multiple graphs in one single page?
A common way to help the performance would be to decrease the number of Data Points that you show at once. But, as you mentioned, dynamic graphs are computationally expensive to have.
I hope this helps you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.