2023-11-24 7:32 AM
Hi Gfx Team,
When I try to call Line::setLine ()
touchgfx::Line line {};
line.setLine ( .5f, 7, 5.5, 7 );my MSVC compiler says
Error C2672 'touchgfx::Line::setLine': no matching overloaded function found
Error C2784 'void touchgfx::Line::setLine(T,T,T,T)': could not deduce template argument for 'T' from 'int'
Error C2782 'void touchgfx::Line::setLine(T,T,T,T)': template parameter 'T' is ambiguous
Error (active) E0304 no instance of function template "touchgfx::Line::setLine" matches the argument list
I tried and it seems to help when Line::setLine () is defined like this:
template <typename T1, typename T2, typename T3, typename T4>
void setLine(T1 startX, T2 startY, T3 endX, T4 endY)
{
setStart(startX, startY);
setEnd(endX, endY);
}
template <typename T1, class T2>
void setStart(T1 x, T2 y)
{
setStart(CWRUtil::toQ5<T1>(x), CWRUtil::toQ5<T2>(y));
}
etc.
Do you think you could change function templates to this form ?
Thanks
Ferro
Solved! Go to Solution.
2024-02-06 6:51 AM
Hello @ferro ,
I see the issue you are mentioning, but changing that template variable will require more treatment than what it appears. Therefore, I would suggest using all floating numbers in your case, so it would be:
line.setLine ( 0.5f, 7.0f, 5.5f, 7.0f );
I hope this helps you,
Good luck
2024-02-06 6:51 AM
Hello @ferro ,
I see the issue you are mentioning, but changing that template variable will require more treatment than what it appears. Therefore, I would suggest using all floating numbers in your case, so it would be:
line.setLine ( 0.5f, 7.0f, 5.5f, 7.0f );
I hope this helps you,
Good luck
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.