2024-05-09 7:28 AM
Hi I have a scrollable container inside a swipe container and i need to check when the drag is horizontal and when it's vertical so that I can channel the event to the one i want it to handle with, this was discussed and resolved in this post:
https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/swiping-and-scrolling/td-p/238053
But I have tried to implement it, changing the variable names but I have the following problems
This is how i have declared the functions in the view.hpp
class VacuumFunctionsView : public VacuumFunctionsViewBase
{
public:
VacuumFunctionsView();
virtual ~VacuumFunctionsView() {}
virtual void setupScreen();
virtual void tearDownScreen();
virtual void customizeToggles();
protected:
bool isListClicked;
virtual void handleClickEvent(const ClickEvent& evt){}
virtual void handleDragEvent(const DragEvent& evt){}
virtual void handleGestureEvent(const GestureEvent& evt){}
And this is how i have implemented it in the cpp
void VacuumFunctionsView::handleClickEvent(const ClickEvent& evt)
{
if (evt.getType() == ClickEvent::PRESSED)
{
if(scrollProducts.getAbsoluteRect().intersect(evt.getX(), evt.getY()))
{
isListClicked = true;
}
}
else if (evt.getType() == ClickEvent::RELEASED)
{
dragType = NONE;
}
if(dragType != VERTICAL) //The swipe container should handle the event
{
swipeContainer.handleClickEvent(evt);
}
VacuumFunctionsViewBase::handleClickEvent(evt);
}
void VacuumFunctionsView::handleDragEvent(const DragEvent& evt)
{
if(isListClicked)
{
isListClicked = false;
if(abs(evt.getDeltaY()) < abs(evt.getDeltaX()))
{
dragType = HORIZONTAL;
}
else
{
dragType = VERTICAL;
}
}
else
{
if(dragType == HORIZONTAL) //The swipe container should handle the event
{
swipeContainer.handleDragEvent(evt);
}
else //The scroll container or the view should handle the event
{
VacuumFunctionsViewBase::handleDragEvent(evt);
}
}
}
void VacuumFunctionsView::handleGestureEvent(const GestureEvent& evt)
{
if(dragType == HORIZONTAL) //The swipe container should handle the event
{
swipeContainer.handleGestureEvent(evt);
}
else //The scroll container or the view should handle the event
{
VacuumFunctionsViewBase::handleGestureEvent(evt);
}
}
Solved! Go to Solution.
2024-05-11 12:12 PM
Hello Iñaki
Its bit difficult to understand completely your problem, but lets try.
Even though I have declared the classes in my view.hpp it says that the cpp cant see them, so i was wondering that maybe im doing it wrong, also i have tried to look for the functions in the upwards inheritance of the viewbase class but i couldnt find it, i saw that the classes like container do have it as they come from drawable.
@Iñaki_Bidasoro wrote:
Seems that you are allready defining functions to empty... test like this in .hpp:
virtual void handleClickEvent(const ClickEvent& evt);
virtual void handleDragEvent(const DragEvent& evt);
virtual void handleGestureEvent(const GestureEvent& evt);
//Instead of
// virtual void handleClickEvent(const ClickEvent& evt){}
// virtual void handleDragEvent(const DragEvent& evt){}
// virtual void handleGestureEvent(const GestureEvent& evt){}
@Iñaki_Bidasoro wrote:
- the variable dragType is not found either, and this one I couldnt find anywhere, so maybe he created it but im not sure as it looks like a touchgfx variable.
For me it looks like just user-defined enumerated variable where dragging state is stored so I would add something like this to view.hpp
enum dragTypeEnum
{
NONE,
HORIZONTAL,
VERTICAL
};
dragTypeEnum dragType=NONE;Maybe this helps you:thumbs_up:
Br JTP
2024-05-11 12:12 PM
Hello Iñaki
Its bit difficult to understand completely your problem, but lets try.
Even though I have declared the classes in my view.hpp it says that the cpp cant see them, so i was wondering that maybe im doing it wrong, also i have tried to look for the functions in the upwards inheritance of the viewbase class but i couldnt find it, i saw that the classes like container do have it as they come from drawable.
@Iñaki_Bidasoro wrote:
Seems that you are allready defining functions to empty... test like this in .hpp:
virtual void handleClickEvent(const ClickEvent& evt);
virtual void handleDragEvent(const DragEvent& evt);
virtual void handleGestureEvent(const GestureEvent& evt);
//Instead of
// virtual void handleClickEvent(const ClickEvent& evt){}
// virtual void handleDragEvent(const DragEvent& evt){}
// virtual void handleGestureEvent(const GestureEvent& evt){}
@Iñaki_Bidasoro wrote:
- the variable dragType is not found either, and this one I couldnt find anywhere, so maybe he created it but im not sure as it looks like a touchgfx variable.
For me it looks like just user-defined enumerated variable where dragging state is stored so I would add something like this to view.hpp
enum dragTypeEnum
{
NONE,
HORIZONTAL,
VERTICAL
};
dragTypeEnum dragType=NONE;Maybe this helps you:thumbs_up:
Br JTP
2024-05-13 1:28 AM
Thank you that was it!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.