2024-04-29 6:01 AM - edited 2024-04-29 6:30 AM
"I've tried reinstalling, but I'm still encountering the following errors:
2024-04-29 11:22 PM
Hello @mimiRJay ,
First, Welcome to the TouchGFX forum.
Can you tell me, which version of windows you are using ?
Regards,
2024-04-30 4:40 AM
Hello @LouisB。
windows 10
2024-05-03 2:13 AM
Hi @mimiRJay,
In the 4.16, by TCP/IP issue, you are talking of not being able to download Demos ? That's a known issue that is not related to Touch GFX directly.
In the 4.20 what's the generator error ? And in 4.23 can you check your proxy and also retry it ?
Regards,
2024-05-12 2:25 AM
Hello @LouisB
When using the 'Generate Code' feature, an error occurred showing 'Generate Code Failed' (TouchGFX 4.20.0).
When using Generate Code functionality, encountering an error related to 'SSL/TLS secure channel' (TouchGFX 4.16.0).
When attempting to download certain examples, I'm unable to download them.(TouchGFX 4.23.2)
displays
~~~
Sorry - something unexpected has happened which caused an error to occur in the Designer.
For more information, see the log file located at: C:\Users\User\AppData\Roaming\TouchGFX-4.23.2\TouchGFXDesigner.log
Please consider reporting this bug and steps to reproduce it at the TouchGFX Help Center so it can be fixed in a future version.
You can find the Help Center here: https://community.st.com/touchgfx
Error: Object reference not set to an instance of an object.
~~~
2024-05-12 3:57 AM
Known Issues | TouchGFX Documentation start with visual C redist
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.