STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Move pages at any time in touchgfx

I am using page 10 in touchgfx, and if an internal error occurs on any page, I would like to go to the error page. Is there a simple way to implement this?(Because of the MVP pattern, it seems like conditions need to be implemented on every page)

kimsj by Associate
  • 1338 Views
  • 1 replies
  • 0 kudos

Resolved! Don't know how to inherit handleClickEvent()

Hi I have a scrollable container inside a swipe container and i need to check when the drag is horizontal and when it's vertical so that I can channel the event to the one i want it to handle with, this was discussed and resolved in this post:https:/...

TouchGFX Usage Issues

"I've tried reinstalling, but I'm still encountering the following errors:TouchGFX 4.23.2: Unable to download Demo project and Generate Code.TouchGFX 4.20.0: Can download Demo project but unable to Generate Code.TouchGFX 4.16.0: Able to Generate Code...

mimiRJay by Associate II
  • 3515 Views
  • 5 replies
  • 0 kudos

Resolved! TouchGFX Designer doesn't list all Win11 fonts

Hi,I don't understand why TouchGFX Designer can't show some windows fonts.I download from internet the font called "GoogleSans-Medium.ttf" and I installed on Win11 correctly.OpenOffice and others PC softwares allow to me to use it without any problem...

MPast.1 by Senior II
  • 2622 Views
  • 2 replies
  • 0 kudos

Resolved! TouchGFX Color Issue with QSPI Flash

I am currently working on a TouchGFX project with an H7 custom board with QSPI external flash and SDRAM.I am able to get the display working properly when not using the external flash.The external flash has been tested separately by writing to it & u...

wlynn777 by Associate III
  • 6080 Views
  • 5 replies
  • 1 kudos

Resolved! How to update textArea value in custom container?

Hi all,I have create a custom container named "tableLine":And using the "tableLine", I make a "table":in "tableLine.cpp", I write the following code:void tableLine::setLineContent(tableItem_t* item) { Unicode::snprintf(txtIDBuffer, TXTID_SIZE, "%s",...

Junde_0-1715329850891.png Junde_1-1715329996975.png Junde_2-1715330427148.png
Junde by Senior III
  • 1905 Views
  • 1 replies
  • 2 kudos

Resolved! How to use TouchGFX,STM32cubeIDE, STM32cubeMX these three software to produce a simple GUI program?

Hello everyone programmers, I am a beginner of stm32, and now I have a few questions for you:Question 1: I want to know how to use TouchGFX STM32cubeIDE and STM32cubeMX to make a simple GUI program? Tell me how these three pieces of software work tog...

judy by Associate II
  • 4071 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.