2024-05-08 5:14 PM
I am using page 10 in touchgfx, and if an internal error occurs on any page, I would like to go to the error page. Is there a simple way to implement this?
(Because of the MVP pattern, it seems like conditions need to be implemented on every page)
2024-05-13 8:40 AM
Hello @kimsj ,
Welcome to the community!
I have trouble understanding what you mean by
I am using page 10 in touchgfx
Have you made a TouchGFX Designer project using 10 screens ?
In that case, if you encounter an error (hardfault or unexpected display behavior I guess), then the issue is on the currently displayed screen or the common files (frontendApplication, model, æodelListener, etc) because the screens that are not displayed currently are not running any code.
Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.