STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Remove loader to fast debug

Hi all,I'm building a custom board with touchgfx and QSPI resources.Everything work well!I would like to know how is possible to remove loader to fast the debugger session: the external resource need more than 4Mbytes and loader everytime I start a d...

MPast.1 by Senior II
  • 2884 Views
  • 7 replies
  • 0 kudos

STM32IDE+TouchGFX can't start.

I try to connect LCD by SPI to Nucleo-767 and TouchGFX. LCD screen work perfect and I could draw on it without a problem, but I stuck with TouchGFX. I found that void TouchGFXHAL::flushFrameBuffer never call.Check this video - https://youtu.be/1UhEx7...

TouchGFX with 16 bit 8080 LCD interface

Hello. We have a need to work with a 16-bit 8080 style LCD interface. Would like to have the benefits of the latest TouchGFX tool (4.16.0) and STM32CubeMX to build quickly and debug our GUI screens. After some investigation, found the following kit w...

Mon2 by Senior III
  • 7132 Views
  • 7 replies
  • 0 kudos

Resolved! DMA2D throws configuration error

Hello, on my STM32H747-DISC1, I had huge issues with DMA2D and CLUT (it was freezing etc).I thought it's because cache maintenance, but anyway after doing everything correctly, DMA is still buggy. Finally I find out, that 90% of my DMA2D executions t...

Resolved! DMA is freezing

Hello, I have my project based on STM32H753I-EVAL with RGB LCD display and SDRAM.I'm using DMA2D to render lines with CLUT L8 (Pulling mode). Basically, I process data for one line (one line have 320 pixels), and then execute it 108 times (for height...

0693W000006GkNqQAK.png 0693W000006GkOjQAK.png 0693W000006GkP3QAK.png

Canvas buffer generated by Designer

Hi,I have allocated memory in external sdram and set buffer using CanvasWidgetRenderer::setupBuffer() method. Generated base class for my view is allocating memory in internal RAM and in constructor is passing it to setupBuffer mehod. How to avoid th...

Luk35 by Associate III
  • 2463 Views
  • 5 replies
  • 0 kudos

Resolved! Memory/Flash usage analysis

Hello,I am looking to perform a similar resource usage as explained here https://support.touchgfx.com/docs/basic-concepts/memory-usage/However, I am wondering if there is a guide that is available using freely available tools to dothe memory analysis...

RReta.1 by Associate III
  • 4374 Views
  • 2 replies
  • 1 kudos

Drivers for VGG128017-C with STM32F769i-eval

I'm new to ST products and am trying to run the LCD_DSI_VideoMode_SingleBuffer example on the Eversion VGG128017-C TFT screen. I get the backlight to turn on, but never see anything. Does anyone know of any specific drivers for the VGG128017 family? ...

DHone.1 by Associate
  • 1180 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.