2021-01-15 9:25 AM
I'm new to ST products and am trying to run the LCD_DSI_VideoMode_SingleBuffer example on the Eversion VGG128017-C TFT screen. I get the backlight to turn on, but never see anything. Does anyone know of any specific drivers for the VGG128017 family?
Thanks
2021-01-21 1:53 AM
Hi @DHone.1 ,
Welcome on ST Community!
The example LCD_DSI_VideoMode_SingleBuffer is developed in a way that it matches the STM32F769I-EVAL hardware configuration.
It will work properly if you use the DSI to HDMI adapter board (B-LCDAD-HDMI1, MB1232) or the B-LCD40-DSI1 daughterboard (MB1166).
Step to follow to run the example are provided in the readme.txt file:
Now that you want to interface a different TFT display, it is required to add VGG128017-C as a new BSP component (under STM32Cube_FW_F7\Drivers\BSP) then adapt the example with these updates.
You can refer to AN4861 LCD-TFT display controller (LTDC) on STM32 MCUs for recommendations on how to use and configure the LTDC peripheral.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.