STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! JPEG encoding issue when using DMA on STM32H7B3

with libjpeg or using hardware in polling, mode compression works fine.but when using DMA image is getting corrupted#include "jpeg_encode.h"   #include "jpeglib.h" #include "jdata_conf.h"   // variables used for dma mode uint32_t YCBCR_Size; uint32_t...

0693W000006I7cbQAC.png 0693W000006I7cWQAS.png 0693W000006I7cRQAS.png
ALamb.314 by Associate II
  • 2963 Views
  • 2 replies
  • 2 kudos

GEsture Event not works

My HPP#ifndef PRINT_PROGRESS_SCREENVIEW_HPP #define PRINT_PROGRESS_SCREENVIEW_HPP   #include <gui_generated/print_progress_screen_screen/PRINT_PROGRESS_ScreenViewBase.hpp> #include <gui/print_progress_screen_screen/PRINT_PROGRESS_ScreenPresenter.hpp>...

EEuge by Senior
  • 2438 Views
  • 8 replies
  • 0 kudos

Use STM32 to receive HDMI data from receive IC

HelloI have an Idea that involves getting video from a PC to an MCU or equivalent. I'm thinking to use ADV7611 to do the deserialization and use its output with the DCMI interface on an STM32. For me it seems like this would be possible as many of th...

Jaxc by Associate
  • 862 Views
  • 0 replies
  • 0 kudos

Max DCMI pixel clock on H7?

Hi all,I'm planning to interface a DCMI camera with an STM32H743 running at 400MHz SYSCLK. What is the greatest pixel clock rate I can reliably use? The reference manual says "The maximum DCMI_PIXCLK period must be higher than 2.5 HCLK periods". Sinc...

Working with a display using DSI in a video mode

Good day!I try to work with 1.3 TFT LCD 320RGB x 320 with ST7796DW driver using STM32L4R9ZG DSI in a video mode. I try to initialize the display using HAL_DSI_ShortWrite and HAL_DSI_LongWrite functions. But after only 3 commands (doesn't matter HAL...

STolm.1 by Associate
  • 1415 Views
  • 1 replies
  • 0 kudos

Resolved! LTDC double buffer

HiI'm using stm32f767 and want to use LTDC with double framebuffer.Can i do this with one sdram?LTDC is fetching data from sdram(front buffer) and i have to prepare the back buffer at the same time(load data from sdcard into sdram)Internal sram capac...

Resolved! Determining the current view

Suppose there are two views: "Screen1" and "Screen2". Depending on which screen is active, we want to do something (like enable or disable an interrupt). Within the Model, what is the proper way to determine which screen is active? Is there an API th...

Chandler by Associate II
  • 3705 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.