STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Using touchgfx without external RAM

I designed a GUI on stm32f746 discovery board and programmed the board successfully and GUI worked perfectly, now I want to redesign the GUI and my programm to be able to use a custom board which doesn't have an external RAMat first I disabled the MX...

ETale.1 by Associate III
  • 11550 Views
  • 26 replies
  • 1 kudos

TouchGFX with STM32F469I-DISCO compiler errors

Running STM32CubeIDE 1.7.0 and TouchGFX 4.18.0.I double click on .project file to invoke STM32CubeIDE.Project for STM32F746G_DISCO compiles and runs ok.Compile errors encountered with STM32F469I-DISCO. Something to do with how the project is imported...

Resolved! Does CubeMX 5.0.0 Ready to Build a TouchGFX Project?

I upgraded my CubeMX to 5.0.0 and installed F4 1.22.0 firmware recently.So, I tried to use CubeMX build a TouchGFX Project that use TrueSTUDIO as IDE.Since I was successful run a STemWin Project as my custom F429IGx board graphic solution.In order to...

0690X000006CSy2QAG.jpg 0690X000006CSy7QAG.jpg
Zhi Pang by Associate III
  • 22043 Views
  • 58 replies
  • 1 kudos

STM32L476 + RGB interface

Hello, everyone!I'm developing smartwatch as a project and I'm planning to use a TFT display which has 18RGB interface. I have STM32L476 at my disposal that doesn't have any embedded LTDC module. Should I change MCU to one that does have LTDC in orde...

Resolved! Question on video widget in TouchGFX new version(4.18.0)

Hi,whenever we are using videos for video widget to upload it was not taken .only it gave output for what they were gave to us as a example video.Any solution please how we can access our videos (that to is in avi format) for video widget in touchgf...

MG.7 by Associate
  • 2372 Views
  • 3 replies
  • 0 kudos

Error in code generation for TouchGFX

Hi,When I generate the code with STM32CubeMX version 6.3 for STM32H747XIHx something like this happens: I have also noticed that when I chose TouchGFX component I am able to use it only with M4 core (this configuration was forced by CubeMX) what is a...

0693W00000GWFLvQAP.png
aroni525 by Associate II
  • 8558 Views
  • 14 replies
  • 0 kudos

TouchGFX 8bpp color format

Hey!I'm having wrong colors issue when drawing shapes with 8 bpp color format. It's clean simulator project with only color format settings changed. How to fix that?Images attached.Thanks

VLau by Associate III
  • 3505 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.